The page you're viewing is for Korean (Korea) region.

Vertiv 영업담당자에게 문의하시면 고객의 고유한 요구에 맞게 복잡한 설계를 구성할 수 있습니다. Vertiv는 대규모 프로젝트에 대한 기술 지침이 필요한 조직에 필요한 지원을 제공할 수 있습니다.

자세히 보기

많은 고객이 Vertiv 리셀러 파트너와 협력하여 IT 애플리케이션을 위한 Vertiv 제품을 구매합니다. 파트너는 다양한 교육을 받고 전문 경험을 보유하고 있으며 Vertiv 제품을 통해 전체 IT 및 인프라 솔루션을 지정, 판매, 지원할 수 있는 독보적인 위치에 있습니다.
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
Challenge

When Secant Technologies, of Kalamazoo, MI, decided to build its own colocation and cloud hosting data center, it wanted a facility that would last 15 to 20 years.

“We set goals for reliability, goals for power efficiency, goals for flexibility and expandability, and we realized as soon as we take over the stewardship of somebody’s data there really is no excuse for that being down,” said Alex Ellingsen, Chief Technology Officer for Secant Technologies.

Strategy

Secant Technologies designed its data center for the highest possible efficiently, reliability, and capacity per rack. Its thermal management configuration, using Liebert DSE free-cooling systems, which allows it to achieve rack densities up to 36kW using perimeter cooling. For low-footprint power protection, it turned to Liebert NX 200kW UPS units operating with flywheel backup.

The Secant Technologies data center has six separate 10-gigabit fiber entrances from carriers and many of those are rings. Reach out to its two other data centers near Detroit, the company can pick up an additional 50 carriers for connectivity to the Cloud.

Download the Case Study
PORTALS
개요
파트너 로그인

언어 & 지역