Sorry, this page isn't available for your location.

The page you're viewing is for Japanese (Japan) region.

Vertivの製造担当者と連携すると、複雑な設計をお客様独自のニーズに合わせて構成することが可能になります。大規模なプロジェクトに関する技術的ガイドが必要な組織に対して、Vertivは十分なサポートを提供いたします。

詳細を見る

Vertiv再販業者パートナーと連携して、多くのお客様がITアプリケーション用のVertiv製品を購入しています。パートナーは、広範なトレーニングと経験を積み、ITおよびインフラに関するソリューション全体をVertiv製品で明確にし、販売、サポートを行うという独自の立場を構築しています。

再販業者を見つける

ご自身に必要なものについて特定済みですか? 便利なオンラインショッピングおよび配送をご希望ですか? 特定のカテゴリーのVertiv製品は、オンライン再販業者を通じて購入可能です。


販売代理店のECサイトを検索

製品選択にサポートが必要ですか? Vertivの有能なスペシャリストにご相談ください。お客様に最適なソリューションをご提案いたします。



Vertivのスペシャリストに問い合わせる

Sorry, this page isn't available for your location.

The page you're viewing is for Japanese (Japan) region.

The new Vertiv™ Liebert® APM Plus is designed for reduced energy use and CO2 emissions

Singapore [November 24, 2022] – Vertiv (NYSE: VRT), a global provider of critical digital infrastructure and continuity solutions, today introduces the new Vertiv™ Liebert® APM Plus, a high-density, modular, and transformer-free uninterruptible power supply (UPS) system that delivers up to 97% efficiency in double conversion mode, and up to 99% efficiency in eco-mode. Available from 50 to 500kW, the Liebert APM Plus is available today throughout Asia, including Australia and New Zealand, and India.

The Liebert APM Plus architecture is designed to optimize energy use and heat dissipation, minimizing the demand and consumption of data center air conditioning systems. The combination of these factors reduces CO2 emissions to a minimum, thus helping data centers to meet environmental compliance standards.

The Liebert APM Plus is an upgrade from the Liebert® APM models, and is ideal for mid-size to large data centers in the telecom, hyperscale and colocation spaces. The Liebert APM Plus features a slimmer body at 600 millimeters, 50% smaller than the previous model without compromising on efficiency. Its smaller footprint, achieved through ultra-high density power modules, makes it ideal for providing power availability to mission-critical applications.

With its built-in FlexPower™ technology, the Liebert APM Plus allows for simple, fast expansion of system capacity with its modular design. Each FlexPower™ module combines scalable power with independent controls to auto-regulate operation, enhancing overall availability.

The Liebert APM Plus features a, hot-swappable design of most of the critical links, supporting low Mean Time To Repair. The robust UPS  can also tolerate temperatures up to 50 degrees Celsius with auto-derating. The system also allows for intelligent monitoring options, compatible with the Vertiv™ Environet™ Alert and the Vertiv™ LIFE™ services.

“The Liebert® APM Plus design shows our commitment to providing our customers with solutions that address the changes of a rapidly growing digital ecosystem,” said Arunangshu Chattopadhyay, director of power product marketing and head of central technical support at Vertiv Asia. “With its flexible design and enhanced features, this UPS is ideal to support the availability needs of today’s customers. Additionally, the Liebert APM Plus’s small footprint makes it ideal for use in Vertiv™ integrated solutions such as  SmartRow™ and SmartAisle™, as well as the Liebert® APT power distribution system.”

Explore more of Vertiv’s UPS solutions at www.Vertiv.com.

 

# # #

 

 

 

About Vertiv

Vertiv (NYSE: VRT) brings together hardware, software, analytics and ongoing services to enable its customers’ vital applications to run continuously, perform optimally and grow with their business needs. Vertiv solves the most important challenges facing today’s data centers, communication networks and commercial and industrial facilities with a portfolio of power, cooling and IT infrastructure solutions and services that extends from the cloud to the edge of the network. Headquartered in Columbus, Ohio, USA, Vertiv employs approximately 24,000 people and does business in more than 130 countries. For more information, and for the latest news and content from Vertiv, visit Vertiv.com.

 

Forward-Looking Statements

This release contains forward-looking statements within the meaning of the Private Securities Litigation Reform Act of 1995, Section 27 of the Securities Act, and Section 21E of the Securities Exchange Act. These statements are only a prediction. Actual events or results may differ materially from those in the forward-looking statement set forth herein. Readers are referred to Vertiv’s filings with the Securities and Exchange Commission, including its most recent Annual Report on Form 10-K and any subsequent Quarterly Reports on Form 10-Q for a discussion of these and other important risk factors concerning Vertiv and its operations. Vertiv is under no obligation to, and expressly disclaims any obligation to, update or alter its forward-looking statements, whether as a result of new information, future events or otherwise.

 

 

CONTACT
Katrina Tirante
T +6326203600 Ext 7666
E Katrina.Tirante@vertiv.com

 

Reinier Dungca
T +6326203600 Ext 7657
E Reinier.Dungca@vertiv.com

PARTNERS
概要
Partner Login

言語と地域