The page you're viewing is for Japanese (Japan) region.

Vertivの製造担当者と連携すると、複雑な設計をお客様独自のニーズに合わせて構成することが可能になります。大規模なプロジェクトに関する技術的ガイドが必要な組織に対して、Vertivは十分なサポートを提供いたします。

詳細を見る

Vertiv再販業者パートナーと連携して、多くのお客様がITアプリケーション用のVertiv製品を購入しています。パートナーは、広範なトレーニングと経験を積み、ITおよびインフラに関するソリューション全体をVertiv製品で明確にし、販売、サポートを行うという独自の立場を構築しています。
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
Avocent® AV100 KVM delivers simple switching solution for local server management

Columbus, Ohio [March 8, 2018] – Vertiv, formerly Emerson Network Power, today introduced the Avocent® AV100 KVM switch, a single-user KVM switch tailored for IT rooms, small data centers, branch offices and other small spaces. Designed specifically for on-site asset management, the Avocent AV100 delivers a simple, cost-effective solution to streamline server access and control. It is available globally.

The Avocent AV100 is available in 4, 8 and 16 port models. All models allow DisplayPort and VGA connections, an important feature as more server manufacturers move to DisplayPort connectivity. They also come with a USB port dedicated for firmware updates. The KVM is designed to support applications that do not allow IP connectivity, eliminating a potential access point for hackers and enhancing network security.

“More businesses are opting to keep their most sensitive servers secure by eliminating IP connectivity to those applications,” said Jay Wirts, vice president and general manager of IT management products at Vertiv. “The Avocent AV100 is designed for these local networks, allowing simplified on-site server selection and asset management and ensuring network security at the KVM switch.”

The Avocent AV100 features touch-button operation, making server selection easier, faster and more intuitive than the traditional single-button scrolling common in most entry-level KVM switches. Coupled with an on-screen display for the 8 and 16-port models, the Avocent AV100 features a best-in-class user interface.

The system can be deployed in desktop or rackmount (0U or 1U) configurations.

For more information on the Avocent AV100 and other KVM solutions from Vertiv, visit www.VertivCo.com.

About Vertiv
Vertiv designs, builds and services critical infrastructure that enables vital applications for data centers, communication networks and commercial and industrial facilities. Formerly Emerson Network Power, Vertiv supports today’s growing mobile and cloud computing markets with a portfolio of power, thermal and infrastructure management solutions including the Chloride®, Liebert®, NetSure™ and Trellis™ brands. Sales in fiscal 2016 were $4.4 billion. For more information, visit VertivCo.com.

CONTACT:
Vince McMorrow
T +614 383 1622
Vince.McMorrow@Fahlgren.com

PARTNERS
概要
Partner Login

言語と地域