High Density Reliable Power Protection for Research and Development in Data Center Lab Operations
23-10-31
Background
End user needed highly efficient, robust power back up and protection for their research and development centers and datacenters which required reliable power solutions that could be easily scaled and maintained along with high power usage effectiveness (PUE). However, the solutions provided by our competitors were not cost effective and utilized more footprint than required. Keeping in mind the stringent project timeline Vertiv could provide the solutions.
Results
- Overall footprint was saved by 30%
- Saved cost of the electrical network infrastructure (Extensive savings in Cable usage)
- Significant savings of capital expenditure (CAPEX) and day to day expenses (OPEX)
- Built in I/P and O/P (optional) switchgear which eliminated external panels.
- Saved time for installation and commissioning (needed 1 week for 3000 kVA installation)
- Reliability and efficiency improvement
| Case Summary | |
|---|---|
| Location: |
Hyderabad, India |
| Critical Need: |
Ensure the availability of critical research and development labs and datacenters while improving energy efficiency within the existing data center footprint in order to meet growing demand without a physical expansion |
| Vertiv Solution: |
|