Vertiv™ Liebert® GXT RT+ UPS addresses all categories of power anomalies, offers intelligent and economical operation
Costa Rica, San Jose – [September 7, 2021] Vertiv (NYSE: VRT), a global provider of digital critical infrastructure and continuity solutions, has introduced the rack/tower convertible Vertiv™ Liebert® GXT RT+ uninterruptible power supply system (UPS). The compact UPS is powerful, intelligent, efficient and reliable, an ideal solution for the protection of high-performance equipment in sectors such as government, banking, telecommunications, health, education, transportation and security, among others. The Liebert® GXT RT +, which was launched in southern cone earlier this year, is now available in Mexico, Colombia, Ecuador, Venezuela, Central America and the Caribbean.
The Liebert GXT RT+ is a double conversion online UPS with the highest output power factor (0.9) in its category and efficiency up to 95%. This UPS comes in four 120V models – 1kVA, 1.5kVA, 2kVA, and 3kVA, with each one offering a least 7 receptacles, an industry best. This cost-effective UPS operates over a wide input voltage window (60 to 150VAC) which helps to preserve the life of the battery.
“Vertiv is constantly delivering simple and practical solutions that save energy, with an efficiency up to 95%, and can be used to support many critical applications. The online topology of Liebert GXT RT+ provides the high availability that edge sites need”, said Victor Medina, product manager for channel solutions in Latin America. “In addition, it is compatible with Vertiv’s management software and optional web/SNMP network cards which allow remote monitoring and control of the UPS.”
The Vertiv Liebert GXT RT+ UPS is an excellent choice for the edge of the network or in locations with limited space, as its compact design enables easy installation in rack or tower configurations. An intuitive liquid crystal display (LCD) provides summary information about the status and configuration of the equipment.
For more information on Liebert® GXT RT+ and Vertiv's complete portfolio of infrastructure management and monitoring solutions, visit Vertiv.com or connect on social media: Facebook, LinkedIn, Instagram and Twitter
About Vertiv
Vertiv (NYSE: VRT) brings together hardware, software, analytics, and ongoing services to ensure its customers’ vital applications run continuously, perform optimally and grow with their business needs. Vertiv solves the most important challenges facing today’s data centers, communication networks and commercial and industrial facilities with a portfolio of power, cooling and IT infrastructure solutions and services that extends from the cloud to the edge of the network. Headquartered in Columbus, Ohio, USA, Vertiv employs approximately 21,000 people and does business in more than 130 countries. For more information, and for the latest news and content from Vertiv, visit Vertiv.com.
Forward-Looking Statements
This release contains forward-looking statements within the meaning of the Private Securities Litigation Reform Act of 1995, Section 27 of the Securities Act, and Section 21E of the Securities Exchange Act. These statements are only a prediction. Actual events or results may differ materially from those in the forward-looking statement set forth herein. Readers are referred to Vertiv’s filings with the Securities and Exchange Commission, including its most recent Annual Report on Form 10-K/A and any subsequent Quarterly Reports on Form 10-Q for a discussion of these and other important risk factors concerning Vertiv and its operations. Vertiv is under no obligation to, and expressly disclaims any obligation to, update or alter its forward-looking statements, whether as a result of new information, future events or otherwise.
CONTACT
Ivis Fernandez
P +3053355883