Sorry, this page isn't available for your location.

The page you're viewing is for English (EMEA) region.

Working with our Vertiv Sales team enables complex designs to be configured to your unique needs. If you are an organization seeking technical guidance on a large project, Vertiv can provide the support you require.

Learn More

Many customers work with a Vertiv reseller partner to buy Vertiv products for their IT applications. Partners have extensive training and experience, and are uniquely positioned to specify, sell and support entire IT and infrastructure solutions with Vertiv products.

Find a Reseller

Already know what you need? Want the convenience of online purchase and shipping? Certain categories of Vertiv products can be purchased through an online reseller.


Find an Online Reseller

Need help choosing a product? Speak with a highly qualified Vertiv Specialist who will help guide you to the solution that is right for you.



Contact a Vertiv Specialist

Sorry, this page isn't available for your location.

The page you're viewing is for English (EMEA) region.

Vertiv™ Integrated Thermal Chain:
The thermal backbone of AI

Not just cooling products. Vertiv delivers end-to-end cooling architecture
engineered for AI-scale efficiency, uptime, and scalability.

Download the eBook Contact us

AI and high-density compute are reshaping data centers faster than traditional cooling can keep up.

AI-driven infrastructure has pushed data centers beyond the limits of traditional cooling. What was once gradual and predictable has become a surge of density, speed, and complexity. These pressures are reshaping cooling into the critical path for uptime and performance, and they manifest in five intensifying challenges:

  • Density: Racks climbing from 5–10 kW to 100 kW+
  • Speed: Capacity must deploy ahead of technology cycles
  • Scale: From pods to gigawatt-scale data centers
  • Complexity: Hybrid air/liquid systems with increasing interfaces
  • Load profile: Dynamic, synchronous workloads requiring 24/7 uptime

The Vertiv™ Integrated Thermal Chain is engineered to meet these challenges head-on — delivering validated, end-to-end architectures that support reliability, scalability, and efficiency for AI infrastructure.

▶ 2 min  –  with George Hannah

Make chilled water work in tight spaces, varied climates, and high-efficiency setups, guided by George Hannah, Senior Director for Global Chilled Water Systems, expert in high-density chilled water systems and lifecycle facility support.

 
▶ 2 min  –  with Enrico Miconi

AI workloads drive power density to extremes, challenging traditional cooling methods. In this Vertiv Tech Talks short, Enrico Miconi, Senior Manager of Product Management for Global Chilled Water Solutions at Vertiv, explains how data centers are evolving with hybrid cooling strategies that combine air and liquid systems.

 
▶ 2 min  –  with Nicola Gattolin

Data centers operate across diverse climates, regulations, and infrastructure constraints. In this Vertiv™ Tech Talks short, Nicola Gattolin, Global Product Manager for Chilled Water Systems at Vertiv, discusses how global cooling strategies must adapt to regional requirements while maintaining consistent performance and reliability.

 
▶ 2 min  –  with Madeline Hoffman

Madeline Hoffman, Offering Specialist at Vertiv, explains how optimizing chilled water temperatures, improving free cooling utilization, and aligning system components can reduce energy consumption and total cost of ownership. By enabling higher operating temperatures, systems can extend free cooling hours, reduce compressor use, and improve overall efficiency.

 

Vertiv delivers integrated thermal architectures across the full cooling stack

Cooling performance depends on coordinated operation across the full thermal chain.

AO-Thermal-Management_Web-Image.jpg

The Vertiv™ CoolLoop Trim Cooler represents the building block of an integrated cooling architecture.

16 units in parallel create a 25 MW cooling block, with three additional units as rotating redundancy. The architecture scales to support your critical digital infrastructure and uptime at hyperscale for hyperscalers and AI-driven facilities.

Download one-pagerLearn more

Modular Capabilities

Vertiv™ solutions


Room Cooling

Precision cooling systems designed for modern data center spaces, offering high efficiency and reliability for both raised and non-raised floor environments.

Check out our products


Rack and In-Row Cooling

Compact cooling systems placed within or between racks—delivering efficient airflow for high-density deployments.

Browse our rack and in-row cooling solutions


Liquid Cooling Solutions

High-density cooling systems (rack, ceiling, or floor-mounted) built to support rising power densities in AI and edge environments.

Learn more about liquid cooling


Heat Rejection

Outdoor and indoor units that remove heat from the facility efficiently, supporting thermal performance and energy targets.

Explore heat rejection systems


Outdoor Packaged Systems

Pre-configured cooling units with integrated economization, supporting air and liquid cooling for high-density deployments.


Check out the Vertiv™ CoolPhase Flex Packaged System


Free Cooling Chillers

Chilled water systems that take advantage of ambient conditions to deliver efficient cooling in small to mid-sized environments.

Dive into our free cooling chillers catalog


Evaporative Free Cooling

Air handling systems that combine indirect heat exchange and evaporative cooling, supporting high-efficiency, low-impact thermal strategies for scalable data centers.

Explore evaporative cooling solutions


Thermal Control & Monitoring

Leverage real-time data and system visibility to adapt cooling performance to changing load conditions, improving efficiency and supporting operational goals.

Discover intelligent thermal control

White paper

Evolving refrigerant regulations and applications in data center environments

Know the international protocols, related studies, and technical details of the new refrigerants that led to the countries’ upcoming mandates to use the new low GWP refrigerants.

Download the White paper

Featured products


Vertiv™ CoolPhase Flex

The Vertiv™ CoolPhase Flex is the industry’s first packaged system offering liquid and air cooling for modern data centers.

Learn about Vertiv™ CoolPhase Flex


Vertiv™ CoolPhase CDU

Designed to remove barriers to liquid cooling in air-cooled environments, the Vertiv™ CoolPhase CDU is a liquid-to-refrigerant coolant distribution unit for direct-to-chip and rear door cooling applications that offers easy, cost-effective deployment in any data center.

Learn about Vertiv™ CoolPhase CDU


Vertiv™ CoolPhase Wall

The Vertiv™ CoolPhase Wall is a wall-mount split system cooling solution for small technical rooms, server rooms, and edge computing applications.


Learn about Vertiv™ CoolPhase Wall

Shaping the future of infrastructure

Scaling data center infrastructure demands tight alignment across design, delivery, and operations. Compass Datacenters and Vertiv bring power, cooling, and services into closer coordination.

Contact a Vertiv representative

For technical guidance or solution planning, connect with a Vertiv representative by completing the form.

Partner Login

Language & Location