Sorry, this page isn't available for your location.

The page you're viewing is for English (EMEA) region.

Working with our Vertiv Sales team enables complex designs to be configured to your unique needs. If you are an organization seeking technical guidance on a large project, Vertiv can provide the support you require.

Learn More

Many customers work with a Vertiv reseller partner to buy Vertiv products for their IT applications. Partners have extensive training and experience, and are uniquely positioned to specify, sell and support entire IT and infrastructure solutions with Vertiv products.

Find a Reseller

Already know what you need? Want the convenience of online purchase and shipping? Certain categories of Vertiv products can be purchased through an online reseller.


Find an Online Reseller

Need help choosing a product? Speak with a highly qualified Vertiv Specialist who will help guide you to the solution that is right for you.



Contact a Vertiv Specialist

Sorry, this page isn't available for your location.

The page you're viewing is for English (EMEA) region.

Vertiv Unveils High-Efficiency DC Power System Designed for Next-Generation Network Growth in EMEA

25/11/25

Vertiv™ PowerDirect 7100 Energy hybrid DC power system delivers reliable, alternative energy -ready performance across on-grid, bad-grid, and off-grid environments

London, UK [November 25, 2025] – Vertiv (NYSE: VRT), a global leader in critical digital infrastructure, today introduced the Vertiv™ PowerDirect 7100 Energy, a hybrid-ready DC power system developed to enable telecom and edge operators to strengthen network reliability and accelerate energy transition strategies. The system delivers scalable power with intelligent controls across diverse operating conditions, from stable grids to remote or off-grid sites, giving operators the flexibility to adapt to new energy sources and growing digital demand.

Now available in Europe, the Middle East, and Africa (EMEA), the Vertiv PowerDirect 7100 Energy delivers up to 52 kW of scalable 48 V DC power and achieves up to 98% efficiency. Built on Vertiv’s fourth-generation hybrid architecture, it seamlessly integrates grid, generator, and alternative energy inputs such as solar, wind, or fuel-cell energy to maintain continuous power where grid reliability is limited.

At the core of the system are Vertiv™ solar converters and Vertiv™ modular rectifiers, managed by the Vertiv™ NetSure™ Control Unit (NCU). Together, these components enable advanced load management, remote monitoring, and energy scheduling to maximize performance and extend equipment life.

“The world expects energy efficiency and flexibility with the growth of communications, such as 5G and edge connectivity”, said Dave Wilson, director of global hybrid solutions at Vertiv. “The Vertiv PowerDirect 7100 Energy gives operators a single, intelligent platform capable of adapting to any grid condition, delivering reliable power while supporting the transition to cleaner, more efficient energy strategies.”

Designed for space-constrained and harsh environments, the Vertiv PowerDirect 7100 Energy is available in 500 A, 750 A, and 1000 A configurations for telecom and edge data racks. A front-access design simplifies installation and service, while operating tolerance from –40 °C to +65 °C supports dependable performance in remote or outdoor sites.

The Vertiv™ PowerDirect 7100 Energy expands Vertiv’s global portfolio of Vertiv™ NetSure™ DC power solutions and hybrid energy systems within its comprehensive power train architecture. Combined with Vertiv’s thermal management, IT management, and lifecycle services, it provides a robust foundation for efficient, reliable, and future-ready digital infrastructure.

For more information on the Vertiv PowerDirect 7100 Energy, visit Vertiv.com

About Vertiv

Vertiv (NYSE: VRT) brings together hardware, software, analytics and ongoing services to enable its customers’ vital applications to run continuously, perform optimally and grow with their business needs. Vertiv solves the most important challenges facing today’s data centers, communication networks and commercial and industrial facilities with a portfolio of power, cooling and IT infrastructure solutions and services that extends from the cloud to the edge of the network. Headquartered in Westerville, Ohio, USA, Vertiv does business in more than 130 countries. For more information, and for the latest news and content from Vertiv, visit Vertiv.com.

Forward-looking statements

This release contains forward-looking statements within the meaning of the Private Securities Litigation Reform Act of 1995, Section 27 of the Securities Act, and Section 21E of the Securities Exchange Act. These statements are only a prediction. Actual events or results may differ materially from those in the forward-looking statements set forth herein. Readers are referred to Vertiv’s filings with the Securities and Exchange Commission, including its most recent Annual Report on Form 10-K and any subsequent Quarterly Reports on Form 10-Q for a discussion of these and other important risk factors concerning Vertiv and its operations. Vertiv is under no obligation to, and expressly disclaims any obligation to, update or alter its forward-looking statements, whether as a result of new information, future events or otherwise.

CONTACT

susanna.collins@apodpr.co.uk

Partner Login

Language & Location