Sorry, this page isn't available for your location.

The page you're viewing is for English (EMEA) region.

Working with our Vertiv Sales team enables complex designs to be configured to your unique needs. If you are an organization seeking technical guidance on a large project, Vertiv can provide the support you require.

Learn More

Many customers work with a Vertiv reseller partner to buy Vertiv products for their IT applications. Partners have extensive training and experience, and are uniquely positioned to specify, sell and support entire IT and infrastructure solutions with Vertiv products.

Find a Reseller

Already know what you need? Want the convenience of online purchase and shipping? Certain categories of Vertiv products can be purchased through an online reseller.


Find an Online Reseller

Need help choosing a product? Speak with a highly qualified Vertiv Specialist who will help guide you to the solution that is right for you.



Contact a Vertiv Specialist

Sorry, this page isn't available for your location.

The page you're viewing is for English (EMEA) region.

Vertiv Launches New Free Cooling Evaporative Solution with Low-GWP Refrigerant to Boost Efficiency and Reduce Carbon Footprint for Data Centres in EMEA

25/3/25

Vertiv™ Liebert® EFC allows hyperscale and colocation clients to easily flex between operating modes for zero water waste and utmost efficiency

London, UK [March 25, 2025] – Vertiv (NYSE: VRT), a global provider of critical digital infrastructure and continuity solutions, today announced a significant upgrade of its thermal management product portfolio with the introduction of the next-gen Vertiv™ Liebert® EFC free cooling unit with low-GWP (Global Warming Potential) refrigerant.  The solution is designed to meet stringent environmental standards for data centre applications, including colocation and cloud services, and is now available across Europe, Middle East and Africa (EMEA) with capacities ranging from 150 to 450 kW.

Vertiv Liebert EFC combines the capabilities of indirect air-to-air heat exchange and evaporative cooling principles in a single unit. The innovative patented polymer heat exchanger and the new low-GWP inverter driven compressor technology significantly enhance annual efficiency by up to 19% compared to previous technologies, allowing a pPUE (partial Power Usage Effectiveness) as low as 1.05.

One of the standout benefits of the Liebert® EFC is its extreme flexibility. Based on onsite-specific conditions, a live toggling control feature allows users to seamlessly and securely reduce the use of critical resources like power or water via software controls, to leverage the free cooling mode. This flexibility empowers data centre owners to reduce their climate impact while enabling continuous cooling, regardless of site-specific resources. Models are available with full direct expansion (DX) back-up with a remote condenser, to supply the entire cooling capacity without any water requirements - offering full water independence, without impacting reliability.

"As businesses prioritise sustainability strategies, customers are increasingly seeking innovative cooling solutions that reduce resource consumption while offering operational flexibility and resilience," stated Sam Bainborough, vice president, thermal business EMEA at Vertiv. "The Liebert EFC, with its game-changing and patented technology, addresses these needs with a flexible system that delivers an entirely new experience for the customer, maximising time using free cooling and leveraging the natural power of evaporation.”

The new Liebert EFC complies with current global regulations and bans (EU F-Gas regulation 2024/573, and IPCC AR4), offering a turnkey solution engineered for future scalability, easy maintenance, and durability. The polymer design offers improved corrosion resistance and also allows a wider range of water qualities during operation when compared to an aluminium heat exchanger. At the core of this cutting-edge solution is Vertiv™ Liebert® iCOM™ and its control algorithms, which manage automatic transitions between the most suitable working modes, enabling use of the preferred cooling source. The controls also enable seamless coordination of units, allowing them to function as a unified system, enhancing cooling continuity and reliability without the need for an additional plant management system. 

For more information on the Vertiv™ Liebert® EFC or other Vertiv power and thermal management solutions, including direct-to-chip, immersion (coming soon in EMEA), chilled water, direct expansion, edge and system control technologies, visit Vertiv.com.

About Vertiv

Vertiv (NYSE: VRT) brings together hardware, software, analytics and ongoing services to enable its customers’ vital applications to run continuously, perform optimally and grow with their business needs. Vertiv solves the most important challenges facing today’s data centres, communication networks and commercial and industrial facilities with a portfolio of power, cooling and IT infrastructure solutions and services that extends from the cloud to the edge of the network. Headquartered in Westerville, Ohio, USA, Vertiv does business in more than 130 countries. For more information, and for the latest news and content from Vertiv, visit Vertiv.com.

Forward-Looking Statements

This release contains forward-looking statements within the meaning of the Private Securities Litigation Reform Act of 1995, Section 27 of the Securities Act, and Section 21E of the Securities Exchange Act. These statements are only a prediction. Actual events or results may differ materially from those in the forward-looking statement set forth herein. Readers are referred to Vertiv’s filings with the Securities and Exchange Commission, including its most recent Annual Report on Form 10-K and any subsequent Quarterly Reports on Form 10-Q for a discussion of these and other important risk factors concerning Vertiv and its operations. Vertiv is under no obligation to, and expressly disclaims any obligation to, update or alter its forward-looking statements, whether as a result of new information, future events or otherwise.

MEDIA CONTACT

Susanna Collins
T +44(0)7872 558593
E susanna.collins@apodpr.co.uk

Partner Login

Language & Location