Sorry, this page isn't available for your location.

The page you're viewing is for English (EMEA) region.

Working with our Vertiv Sales team enables complex designs to be configured to your unique needs. If you are an organization seeking technical guidance on a large project, Vertiv can provide the support you require.

Learn More

Many customers work with a Vertiv reseller partner to buy Vertiv products for their IT applications. Partners have extensive training and experience, and are uniquely positioned to specify, sell and support entire IT and infrastructure solutions with Vertiv products.

Find a Reseller

Already know what you need? Want the convenience of online purchase and shipping? Certain categories of Vertiv products can be purchased through an online reseller.


Find an Online Reseller

Need help choosing a product? Speak with a highly qualified Vertiv Specialist who will help guide you to the solution that is right for you.



Contact a Vertiv Specialist

Sorry, this page isn't available for your location.

The page you're viewing is for English (EMEA) region.

Vertiv Upgrades Pre-Engineered Data Centre Solution for Edge Computing in EMEA to Promote Energy Efficiency and Faster Onsite Deployment

9/4/25

New Vertiv™ SmartAisle™ with integrated monitoring and high-efficiency power and cooling helps reduce costs and energy consumption

London, UK [April 9, 2025] – Vertiv (NYSE: VRT), a global provider of critical digital infrastructure solutions and the leading provider of the full suite of power train and thermal chain solutions, today announced a significant upgrade to its Vertiv™ SmartAisle™ solution, designed specifically for edge computing applications up to 180 kW.

Now available across Europe, the Middle East, and Africa (EMEA), this complete pre-engineered system combines power, cooling, racks, and advanced management and monitoring capabilities in a single integrated unit, designed to simplify and quicken edge computing deployments. In line with the European Union Energy Efficiency Directive (EED) the system provides energy efficient operation and includes power usage effectiveness (PUE) monitoring to help organisations track operations alongside their responsible business goals.

"The upgraded Vertiv™ SmartAisle™ really changes the game when it comes to effective and successful edge deployments", said Giuseppe Leto, senior director IT systems business at Vertiv in EMEA. "We've made it easier, faster, and more cost-effective for businesses to scale and grow their IT operations. The pre-engineered system eliminates the traditional challenges of planning of multiple equipment installations and logistics while providing customers a complete, reliable end-to-end solution that allows data centre operators to monitor energy efficiency requirements following the latest EU regulations.”

The embedded Vertiv™ RDU501 intelligent infrastructure management appliance allows data centre operators to control system operations in real-time 24/7, offering a consolidated and easy to use monitoring and management platform. In addition, the Vertiv approach to pre-engineered, edge smart solutions helps organisations reduce planning, design, and site preparation time by up to 80% while lowering deployment costs by up to 30% compared to a brick-and-mortar alternative, while the integration of all components is designed to achieve up to 20% higher energy efficiency compared to industry averages[1].

Vertiv SmartAisle is part of Vertiv’s growing portfolio of flexible, fully pre-engineered modular solutions. The system is available as standard in four different reference designs, with the ability to scale up to 180kW IT load and features N+1 redundancy for both power and cooling systems.

Key features and benefits include:

  • Advanced 24/7 monitoring of energy consumption and capacity management
  • Precise environmental monitoring with six sensors per server rack
  • High efficiency, modular uninterruptible power supply (UPS) systems
  • Power distribution through power bars or floor-mounted PDUs
  • Integrated power monitoring via rack-mounted power distribution units (rPDU)
  • Adaptive direct expansion cooling system with 20-100% modulating capacity
  • Enhanced thermal efficiency through cold aisle containment
  • Advanced physical security with e-handles and IP cameras
  • Scalable architecture enabling standardised deployment across multiple edge sites

For more information about Vertiv SmartAisle, read the blog post and visit Vertiv.com.

About Vertiv

Vertiv (NYSE: VRT) brings together hardware, software, analytics and ongoing services to enable its customers’ vital applications to run continuously, perform optimally and grow with their business needs. Vertiv solves the most important challenges facing today’s data centres, communication networks and commercial and industrial facilities with a portfolio of power, cooling and IT infrastructure solutions and services that extends from the cloud to the edge of the network. Headquartered in Westerville, Ohio, USA, Vertiv does business in more than 130 countries. For more information, and for the latest news and content from Vertiv, visit Vertiv.com.

Forward-Looking Statements

This release contains forward-looking statements within the meaning of the Private Securities Litigation Reform Act of 1995, Section 27 of the Securities Act, and Section 21E of the Securities Exchange Act. These statements are only a prediction. Actual events or results may differ materially from those in the forward-looking statements set forth herein. Readers are referred to Vertiv’s filings with the Securities and Exchange Commission, including its most recent Annual Report on Form 10-K and any subsequent Quarterly Reports on Form 10-Q for a discussion of these and other important risk factors concerning Vertiv and its operations. Vertiv is under no obligation to, and expressly disclaims any obligation to, update or alter its forward-looking statements, whether as a result of new information, future events or otherwise. 

MEDIA CONTACT

Susanna Collins
T +44 (0)7872 558593
E susanna.collins@apodpr.co.uk


[1] Reference: Global average PUE as reported by the Uptime Institute in 2024

Partner Login

Language & Location