The page you're viewing is for English (EMEA) region.

Working with our Vertiv Sales team enables complex designs to be configured to your unique needs. If you are an organization seeking technical guidance on a large project, Vertiv can provide the support you require.

Learn More

Many customers work with a Vertiv reseller partner to buy Vertiv products for their IT applications. Partners have extensive training and experience, and are uniquely positioned to specify, sell and support entire IT and infrastructure solutions with Vertiv products.

Find a Reseller

Already know what you need? Want the convenience of online purchase and shipping? Certain categories of Vertiv products can be purchased through an online reseller.


Find an Online Reseller

Need help choosing a product? Speak with a highly qualified Vertiv Specialist who will help guide you to the solution that is right for you.



Contact a Vertiv Specialist

The page you're viewing is for English (EMEA) region.

Vertiv adds new direct expansion cooling unit to enable carbon footprint reduction

26/6/24

Vertiv™ Liebert® PDX family expands to utilise low-GWP and non-flammable refrigerant in EMEA

London, UK [26 June, 2024] – Vertiv (NYSE: VRT), a global provider of critical digital infrastructure and continuity solutions, today introduced the new, highly efficient Vertiv™ Liebert® PDX-PAM direct expansion perimeter units with low global warming potential (GWP) and non-flammable R513A refrigerant. Available now in Europe, Middle East and Africa (EMEA), the system is designed to operate with an eco-friendly refrigerant (as compared to legacy refrigerants) to enable increased efficiency, reliability and maximum flexibility of installation.

Liebert® PDX-PAM allows data centre owners to comply with the EU F-Gas Regulation 2024/573 and enables their pressing sustainability goals. The non-flammable R513A refrigerant provides up to a 70% GWP reduction when compared to the traditional R410A, without compromising safety or reliability. No additional safety devices are required, as is the case for units using flammable refrigerants, enabling reduced installation costs and CAPEX.

"In an era where efficiency and reliability are paramount, we recognise the urgent need for eco-friendly alternatives to stay ahead of regulatory requirements and provide our customers with state-of-the-art innovations,” stated Karsten Winther, president for Vertiv in Europe, Middle East and Africa. “With this new solution, we're not just addressing our customers' current sustainability objectives; we're actively innovating and advancing the future of cooling technology and setting new heights for efficiency and reliability."

Liebert PDX-PAM is available from 10 kW to 80 kW with a wide range of airflow configurations, options and accessories, making the unit easily adaptable to various installation needs, from small to medium data centres including edge computing applications, UPS and battery rooms. In conjunction with the Liebert PDX-PAM units, a wide choice of cooling solutions is available for managing heat rejection externally, depending on the specific system configuration.

Vertiv is leading in innovation and raising the technology threshold with Liebert® PDX-PAM , a low-GWP, non-flammable R513A refrigerant solution with inverter-driven brushless motor compressors, staged coil design with an innovative patent-pending filter, electronic expansion valves and state-of-the-art electronically commutated (EC) fans, all included as standard features. The integrated Vertiv™ Liebert® iCOM™ controller enables seamless synchronisation of these components, allowing complete modulation of performance. This way, the Liebert® PDX-PAM unit can adapt to changing operating conditions and heat load efficiently and reliably. The full continuous modulation capability significantly reduces the annual power consumption, resulting in a more cost-effective solution, thanks to the enhanced part load efficiency and precise monitoring of the machine's operation, facilitating performance tracking and more timely and effective maintenance, thereby creating opportunities for predictive maintenance actions.

“The introduction of low GWP refrigerants for direct expansion systems marks a significant advancement in sustainable air-cooling technology,” said Lucas Beran, research director at Dell’Oro Group. By utilising low-GWP and non-flammable refrigerants, Vertiv complies with EU F-Gas Regulation requirements and aims to reduce carbon footprints without compromising on safety or efficiency. This innovation is significant for data centre operators aiming to achieve their sustainability goals while maintaining high operational standards." For more information on the Vertiv™ Liebert® PDX-PAM direct expansion perimeter units with R513A low-GWP refrigerant or other Vertiv solutions, visit Vertiv.com.

About Vertiv

Vertiv (NYSE: VRT) brings together hardware, software, analytics and ongoing services to enable its customers’ vital applications to run continuously, perform optimally and grow with their business needs. Vertiv solves the most important challenges facing today’s data centres, communication networks and commercial and industrial facilities with a portfolio of power, cooling and IT infrastructure solutions and services that extends from the cloud to the edge of the network. Headquartered in Westerville, Ohio, USA, Vertiv does business in more than 130 countries. For more information, and for the latest news and content from Vertiv, visit Vertiv.com.

Forward-Looking Statements

This release contains forward-looking statements within the meaning of the Private Securities Litigation Reform Act of 1995, Section 27 of the Securities Act, and Section 21E of the Securities Exchange Act. These statements are only a prediction. Actual events or results may differ materially from those in the forward-looking statement set forth herein. Readers are referred to Vertiv’s filings with the Securities and Exchange Commission, including its most recent Annual Report on Form 10-K and any subsequent Quarterly Reports on Form 10-Q for a discussion of these and other important risk factors concerning Vertiv and its operations. Vertiv is under no obligation to, and expressly disclaims any obligation to, update or alter its forward-looking statements, whether as a result of new information, future events or otherwise.

MEDIA CONTACT

Susanna Collins
T +44(0)7872 558593
E susanna.collins@apodpr.co.uk

Partner Login

Language & Location