The page you're viewing is for English (Canada) region.

Working with our Vertiv Sales team enables complex designs to be configured to your unique needs. If you are an organization seeking technical guidance on a large project, Vertiv can provide the support you require.

Learn More

Many customers work with a Vertiv reseller partner to buy Vertiv products for their IT applications. Partners have extensive training and experience, and are uniquely positioned to specify, sell and support entire IT and infrastructure solutions with Vertiv products.

Find a Reseller

Already know what you need? Want the convenience of online purchase and shipping? Certain categories of Vertiv products can be purchased through an online reseller.


Find an Online Reseller

Need help choosing a product? Speak with a highly qualified Vertiv Specialist who will help guide you to the solution that is right for you.



Contact a Vertiv Specialist

The page you're viewing is for English (Canada) region.

Vertiv launches utility-grade energy storage system to accelerate data center interconnection and grid resilience in North America

25-12-3

The Vertiv™ EnergyCore Grid factory-integrated battery energy storage system (BESS) is designed to accelerate data center interconnection, support AI power demands, and strengthen grid resilience.

COLUMBUS, Ohio [December 03, 2025] – Vertiv (NYSE: VRT), a global leader in critical digital infrastructure, today announced the Vertiv™ EnergyCore Grid, a modular, utility-grade battery energy storage system (BESS) now available in North America. Designed for data centers, education, and large commercial and industrial facilities, the Vertiv EnergyCore Grid delivers reliable, scalable energy storage that strengthens power resilience and accelerates interconnection in grid-constrained environments.

Built for large-scale, grid-interactive applications, the Vertiv EnergyCore Grid integrates lithium iron phosphate (LFP) batteries, a power conversion system (PCS), and energy management system (EMS) controls within a factory-integrated, modular design. This configuration enables fast deployment and flexible performance across a range of use cases, from 1 MW to more than 200 MW, while supporting functions such as peak-demand optimization, load shifting, black-start operation, and ancillary grid services.

With rising demand for AI and high-density computing increasing power consumption worldwide, the Vertiv EnergyCore Grid provides a faster, more flexible path to expand available capacity without waiting for costly utility upgrades. Its skid-based architecture simplifies installation and commissioning, while its integrated controls and modular form factor bring repeatability and scalability to complex energy storage projects.

“With datacenters needing more power to support AI growth, getting a grid interconnection has unfortunately never been more difficult,” said Chris Thompson, global vice president of microgrid solutions at Vertiv. “The Vertiv EnergyCore Grid enables datacenters to provide grid flexibility as well as critical grid ancillary services. This accelerates grid interconnection in an environment where time to first token is paramount.”

Vertiv designed the Vertiv EnergyCore Grid with UL 1973-listed and UL 9540A-tested battery systems and a liquid-cooled, IP55-rated outdoor enclosure to deliver safety and performance in demanding conditions.
The system’s factory-integrated EMS provides real-time visibility and control of distributed energy resources (DERs), enabling intelligent dispatch, market participation, and seamless integration with renewable sources.

Vertiv™ EnergyCore Grid expands Vertiv’s grid to chip portfolio, complementing technologies such as Vertiv™ Trinergy uninterruptible power supply (UPS), Vertiv™ DynaFlex energy systems, and Vertiv™ EnergyCore Li-ion cabinets. Together, these solutions support Vertiv™ 360AI initiatives, enabling customers to build resilient, efficient, and future-ready digital power ecosystems.

For more information about Vertiv EnergyCore Grid, visit Vertiv.com.

About Vertiv

Vertiv (NYSE: VRT) brings together hardware, software, analytics and ongoing services to enable its customers’ vital applications to run continuously, perform optimally and grow with their business needs. Vertiv solves the most important challenges facing today’s data centers, communication networks and commercial and industrial facilities with a portfolio of power, cooling and IT infrastructure solutions and services that extends from the cloud to the edge of the network. Headquartered in Westerville, Ohio, USA, Vertiv does business in more than 130 countries. For more information, and for the latest news and content from Vertiv, visit Vertiv.com.

Forward-looking statements

This release contains forward-looking statements within the meaning of the Private Securities Litigation Reform Act of 1995, Section 27 of the Securities Act, and Section 21E of the Securities Exchange Act. These statements are only a prediction. Actual events or results may differ materially from those in the forward-looking statements set forth herein. Readers are referred to Vertiv’s filings with the Securities and Exchange Commission, including its most recent Annual Report on Form 10-K and any subsequent Quarterly Reports on Form 10-Q for a discussion of these and other important risk factors concerning Vertiv and its operations. Vertiv is under no obligation to, and expressly disclaims any obligation to, update or alter its forward-looking statements, whether as a result of new information, future events or otherwise.

 

CONTACT
Ruder Finn
E 
Vertiv@RuderFinn.com

PORTALS
Partner Login

Language & Location