Vertiv Launches Chilled Water-Based Prefabricated Modular Data Center Solution to Address Growing Computing Demand in North America
23-11-2
The Vertiv™ SmartMod™ Max CW infrastructure solution can scale from 100kW to 200kW of total IT load and up to 24 racks
Columbus, Ohio [November 2, 2023] – Vertiv (NYSE: VRT), a global provider of critical digital infrastructure and continuity solutions, today introduced Vertiv™ SmartMod™ Max CW, a prefabricated modular data center designed to address the growing demand for rapid deployment of compute. This configurable and scalable solution supports up to 200kW of total IT load in a single system and utilizes chilled water cooling for reduced environmental impact and energy efficiency. The solution is now available in North America.
The SmartMod™ Max CW is factory assembled and tested, for faster deployment and reduced on-site preparation and costs compared to traditional data center construction. The system also presents a range of customization options, including power and cooling capacities, number of racks and rack sizes, and module dimensions. This flexibility enables data centers to tailor the solution to meet their specific requirements, from small-scale operations like edge data centers, to mid-size enterprises, government, and healthcare.
Chilled water thermal management is a high efficiency option for data center cooling, and employs low Global Warming Potential (GWP) refrigerants in data center applications. The use of the technology also enables a reduction in electrical energy usage, helping to support lower overall operating costs.
"Digitalization is driving the need for more and higher capacity compute. In parallel, customers are looking for alternatives that take advantage of high efficiency systems. Data centers and other critical applications are looking for ways to deploy capacity quickly to remain competitive. Vertiv™ SmartMod™ Max CW addresses these challenges with a flexible and modular solution,” said Matt Weil, vice president, integrated modular solutions for Vertiv.
Vertiv™ SmartMod™ Max CW incorporates Vertiv™ Liebert® EXM uninterruptible power supply (UPS) system, available in power ratings of 100kW, 150kW, and 200kW; in-row Vertiv™ Liebert® thermal management units with intelligent controls, Vertiv™ Environet™ Alert monitoring system, and integrated fire suppression.
The SmartMod Max CW consists of two 9'6" wide modules that are connected during installation at the site to form the IT and infrastructure enclosure. The installed enclosure has a width of 19' and a height of 10'11". It operates at a voltage of 480VAC, 60Hz. The supporting chiller skid measures 11' 3'' wide x 22' 6'' length.
For more information on the Vertiv SmartMod Max CW and other solutions, visit Vertiv.com.
About Vertiv
Vertiv (NYSE: VRT) brings together hardware, software, analytics and ongoing services to enable its customers’ vital applications to run continuously, perform optimally and grow with their business needs. Vertiv solves the most important challenges facing today’s data centers, communication networks and commercial and industrial facilities with a portfolio of power, cooling and IT infrastructure solutions and services that extends from the cloud to the edge of the network. Headquartered in Westerville, Ohio, USA, Vertiv does business in more than 130 countries. For more information, and for the latest news and content from Vertiv, visit Vertiv.com.
Forward-Looking Statements
This release contains forward-looking statements within the meaning of the Private Securities Litigation Reform Act of 1995, Section 27 of the Securities Act, and Section 21E of the Securities Exchange Act. These statements are only a prediction. Actual events or results may differ materially from those in the forward-looking statements set forth herein. Readers are referred to Vertiv’s filings with the Securities and Exchange Commission, including its most recent Annual Report on Form 10-K and any subsequent Quarterly Reports on Form 10-Q for a discussion of these and other important risk factors concerning Vertiv and its operations. Vertiv is under no obligation to, and expressly disclaims any obligation to, update or alter its forward-looking statements, whether as a result of new information, future events or otherwise.
CONTACT
Sara Steindorf
T +314-982-1725
E sara.steindorf@fleishman.com