The page you're viewing is for English (Canada) region.

Working with our Vertiv Sales team enables complex designs to be configured to your unique needs. If you are an organization seeking technical guidance on a large project, Vertiv can provide the support you require.

Learn More

Many customers work with a Vertiv reseller partner to buy Vertiv products for their IT applications. Partners have extensive training and experience, and are uniquely positioned to specify, sell and support entire IT and infrastructure solutions with Vertiv products.

Find a Reseller

Already know what you need? Want the convenience of online purchase and shipping? Certain categories of Vertiv products can be purchased through an online reseller.


Find an Online Reseller

Need help choosing a product? Speak with a highly qualified Vertiv Specialist who will help guide you to the solution that is right for you.



Contact a Vertiv Specialist

The page you're viewing is for English (Canada) region.

Vertiv simplifies high-density AI infrastructure deployment across data center environments

26-10-26

The new Vertiv™ SmartIT platform is a pre-engineered AI infrastructure solution based on NVIDIA MGX™ and OCP ORV3 architecture

The scalable solution supports deployment in existing enterprise facilities, new builds, commercial spaces, colocation and hyperscale environments without redesign


COLUMBUS, Ohio [October 26, 2026] — Vertiv Holdings Co. (NYSE: VRT), a global leader in critical digital infrastructure, today introduced the Vertiv™ SmartIT solution, a pre-engineered architecture designed to simplify high-density AI deployments for enterprises, research institutions and colocation providers across existing facilities and new data centers.

Previously deployed with NVIDIA to support the NVIDIA DGX™ GB300, the highest-performing, largest-scale AI system available for enterprises, the Vertiv™ SmartIT solution integrates rack infrastructure, DC power conversion and distribution, direct-to-chip liquid cooling, in-rack cooling distribution and monitoring in a factory-validated design. By integrating and validating these systems before shipment, Vertiv™ SmartIT helps reduce on-site integration complexity and connects to facility power and cooling infrastructure. The solution is available now for AI deployments globally.

“AI is fundamentally changing the demands placed on data center infrastructure, requiring closer coordination across power, cooling and IT systems to support increasingly complex workloads,” said Scott Armul, Chief Product and Technology Officer at Vertiv. “Vertiv™ SmartIT reflects our approach to solving that challenge by bringing these disciplines together in a factory-validated architecture. By combining Vertiv’s expertise across critical infrastructure, we’re helping customers simplify deployment, build greater consistency into their AI environments and establish a foundation that can evolve alongside their computing needs.”

Vertiv™ SmartIT helps customers address key deployment challenges, including:

  • Deployment timelines compress: Factory validation replaces on-site integration, limiting the commissioning scope to facility connections.
  • Multi-vendor coordination is reduced: Customers benefit from a single order, one partner and one architecture spanning rack, power, cooling and monitoring.
  • Existing spaces become AI-ready: Brownfield enterprise facilities and Class A commercial buildings can support AI-class density without full reconstruction.
  • Scalability becomes repeatable: The same building block supports growth from single rack to multi-rack deployments, without redesign between phases.
  • Operational visibility increases: Integrated leak detection, automated response and continuous monitoring provide visibility from rack to site, with these capabilities built into the solution from day one rather than assembled from separate vendor tools.

Vertiv™ SmartIT is a scalable, pre-engineered infrastructure platform for high-density AI deployments, supporting NVIDIA GB300 NVL72, NVIDIA Vera Rubin NVL72, NVIDIA DGX™ Rubin NVL8 and NVIDIA HGX™ Rubin NVL8 on NVIDIA MGX™ and Open Compute Project (OCP) ORV3 architectures.

Designed to scale from a single rack to multi-rack deployments, it enables customers to deploy and expand AI infrastructure within a common architecture while integrating power, cooling, monitoring and controls. Built-in monitoring, leak detection and support for Redfish, SNMP and Modbus simplify operations, while Vertiv™ Global Services supports deployment, commissioning and lifecycle management.

Vertiv SmartIT can be deployed as part of a broader Vertiv infrastructure architecture, with complementary solutions extending integration and management capabilities beyond the rack. Vertiv™ SmartRun extends integration across the row, while Vertiv™ rack power distribution units (rPDU) provide power distribution and monitoring. Vertiv™ Unify provides integrated monitoring, analytics and controls across power and thermal infrastructure, including leak detection and coordinated response control. Together, these solutions help customers scale from individual Vertiv™ SmartIT deployments to larger AI environments.

Vertiv showcased a Vertiv™ SmartIT with a NVIDIA HGX™ Rubin NVL8 demo unit during NVIDIA GTC Berlin in October, demonstrating an integrated infrastructure architecture designed to support NVIDIA DGX Rubin NVL8 deployments, enabling customers to start at the right scale and expand within a common infrastructure architecture as AI demand grows.

For more information about the Vertiv™ SmartIT and Vertiv’s growing portfolio of power, cooling and IT infrastructure solutions and services, visit Vertiv.com.

About Vertiv Holdings Co.

Vertiv Holdings Co. (NYSE: VRT) brings together hardware, software, analytics and ongoing services to enable its customers’ vital applications to run continuously, perform optimally and grow with their business needs. Vertiv solves the most important challenges facing today’s data centers, communication networks and commercial and industrial facilities with a portfolio of power, cooling and IT infrastructure solutions and services that extends from the cloud to the edge of the network. Headquartered in Westerville, Ohio, USA, Vertiv does business in more than 130 countries. For more information, and for the latest news and content from Vertiv, visit Vertiv.com.

Forward-looking statements

This release contains forward-looking statements within the meaning of the Private Securities Litigation Reform Act of 1995, Section 27 of the Securities Act, and Section 21E of the Securities Exchange Act. These statements are only a prediction. Actual events or results may differ materially from those in the forward-looking statements set forth herein. Readers are referred to Vertiv’s filings with the Securities and Exchange Commission, including its most recent Annual Report on Form 10-K and any subsequent Quarterly Reports on Form 10-Q for a discussion of these and other important risk factors concerning Vertiv and its operations. Vertiv is under no obligation to, and expressly disclaims any obligation to, update or alter its forward-looking statements, whether as a result of new information, future events or otherwise.


CONTACT
Ruder Finn
E 
Vertiv@RuderFinn.com

PORTALS
Partner Login

Language & Location