The page you're viewing is for English (Canada) region.

Working with our Vertiv Sales team enables complex designs to be configured to your unique needs. If you are an organization seeking technical guidance on a large project, Vertiv can provide the support you require.

Learn More

Many customers work with a Vertiv reseller partner to buy Vertiv products for their IT applications. Partners have extensive training and experience, and are uniquely positioned to specify, sell and support entire IT and infrastructure solutions with Vertiv products.

Find a Reseller

Already know what you need? Want the convenience of online purchase and shipping? Certain categories of Vertiv products can be purchased through an online reseller.


Find an Online Reseller

Need help choosing a product? Speak with a highly qualified Vertiv Specialist who will help guide you to the solution that is right for you.



Contact a Vertiv Specialist

The page you're viewing is for English (Canada) region.

Vertiv Introduces High-Capacity DC Distribution Bays With Intelligent Load Management

17-10-17

Systems increase power protection and efficiency through enhanced visibility and control

Columbus, Ohio [October 17, 2017] – Vertiv, formerly Emerson Network Power, today introduced the NetSure™ 8100DB series of DC power distribution systems, bringing increased visibility and intelligent load management to telecom, data center and cable industry power infrastructure facilities. The NetSure 8100DB remotely monitors the power draw on individual breakers/fuses, identifying the equipment being used and enabling load shifts to protect sites from potential overload. Netsure 8100DB is globally available now.

The intelligent load management feature in the NetSure 8100DB is unique in the industry and lets users monitor power performance, identify distribution inefficiencies, and adjust the location of the load to optimize the facility’s power supply and avoid overload. This, in turn, enables more effective thermal management since cooling can follow the load, improving the overall efficiency of the network infrastructure.

“Today’s networks and network facilities demand the flexibility that comes with improved visibility and management capabilities, and those demands are increasing with the advent of software-defined networks,” said Scott Armul, vice president and general manager, DC power and outside plant products, for Vertiv in the Americas. “These environments are more complex than ever, becoming more distributed, and requiring scalable solutions. By enabling virtual provisioning and effective load reallocation, the NetSure 8100DB can help organizations significantly reduce operating costs and minimize risk.”

The NetSure 8100DB delivers up to 300 Amp device monitoring, a significant improvement from the industry standard of 125 Amp, and with six- and eight-panel bay sizes, it offers up to 168 breaker positions. Additionally, remote monitoring and management capabilities can reduce onsite control requirements and service calls.

For more information on the NetSure 8100DB and other communication network solutions from Vertiv, visit www.VertivCo.com.

 

About Vertiv
Vertiv designs, builds and services critical infrastructure that enables vital applications for data centers, communication networks and commercial and industrial facilities. Formerly Emerson Network Power, Vertiv supports today’s growing mobile and cloud computing markets with a portfolio of power, thermal and infrastructure management solutions including the ASCO®, Chloride®, Liebert®, NetSure™ and Trellis™ brands. Sales in fiscal 2016 were $4.4 billion. For more information, visit VertivCo.com.

CONTACT
Vince McMorrow
T +614 383 1622
E Vince.McMorrow@Fahlgren.com

 

PORTALS
Partner Login

Language & Location