Sorry, this page isn't available for your location.

The page you're viewing is for English (ASIA) region.

Working with our Vertiv Sales team enables complex designs to be configured to your unique needs. If you are an organization seeking technical guidance on a large project, Vertiv can provide the support you require.

Learn More

Many customers work with a Vertiv reseller partner to buy Vertiv products for their IT applications. Partners have extensive training and experience, and are uniquely positioned to specify, sell and support entire IT and infrastructure solutions with Vertiv products.

Find a Reseller

Already know what you need? Want the convenience of online purchase and shipping? Certain categories of Vertiv products can be purchased through an online reseller.


Find an Online Reseller

Need help choosing a product? Speak with a highly qualified Vertiv Specialist who will help guide you to the solution that is right for you.



Contact a Vertiv Specialist

Sorry, this page isn't available for your location.

The page you're viewing is for English (ASIA) region.

Vertiv Launches Next-Generation Mid-size UPS System for Critical Applications in Southeast Asia, Australia and New Zealand

March 23, 2021

Vertiv™ Liebert® EXM2 delivers industry-leading performance, reliability and efficiency

Singapore [March 23, 2021] – Vertiv (NYSE: VRT), a global provider of critical digital infrastructure and continuity solutions, today introduces Vertiv™ Liebert® EXM2, a three-phase monolithic uninterruptible power supply (UPS) providing double conversion efficiency up to 97%, which further increases up to 98.8% with the dynamic online mode. With power capacity ranging from 100 to 250 kVA and a compact and flexible footprint, the system is designed for a wide range of applications, including metros and railways, healthcare, light industrial, commercial offices and medium size data centers. It is currently available in Southeast Asia, Australia, and New Zealand.

Liebert EXM2 provides technological advancements that enhance efficiency and reliability, such as intelligent paralleling that optimizes performance at partial load to achieve cost savings,  and three machine-learning-based modes of operation which aid in cutting operating costs and keeping energy dissipation to a minimum. It features Vertiv’s proven dynamic on-line mode that delivers up to 98.8% efficiency whilst ensuring fast transfer output performance and reliability. Moreover, the internal modular fault tolerant design allows for safe, easy and fast installation and service, reducing mean time to repair (MTTR) and maximizing availability.

The latest innovations provide industry-leading efficiency and thus energy savings, significantly reducing the total cost of ownership (TCO) and allowing quick return on investment (ROI). Liebert EXM2 is compatible with lithium-ion batteries (LIB) and tolerates high temperatures up to 50°C, which minimizes cooling needs and overall energy consumption.

Liebert EXM2 offers advanced monitoring, management and diagnostic capabilities through a 9-inch touchscreen panel that enables flexible views and multiple security options. The intelligent controls and communications are compatible with Vertiv LIFE Services, Liebert® Nform, SiteScan™ and the Trellis platform infrastructure monitoring software, as well as third-party battery management systems (BMS) and data center infrastructure management (DCIM) systems.

Liebert® EXM2 replaces the flagship Liebert® EXM and Liebert® NXC models, which have been widely recognized as highly performing UPS systems, supporting thousands of sites and about 1.7 GW of mission-critical loads across the globe. This latest product innovation addresses the growing need of highly reliable and efficient UPS for mid-size applications that enable low latency connection between cloud and edge sites.

“The Liebert EXM2 derives its evolution from our industry-leading series of UPS systems, taking one step further in increasing energy savings and bringing latest technologies to our customers,” says Kyle Keeper, vice president of global AC power for Vertiv. “Our growing investment in research and development means that our engineering teams are continuously innovating our portfolio to deliver state-of-the-art solutions.”

“The Liebert EXM2 is designed to support applications across a wide range of industries, from colocation to manufacturing and transportation market segments. With its fault-tolerant design and small footprint, the Liebert EXM2 ensures maximum efficiency and availability, addressing our customers’ evolving requirements in their digital space. We are excited to launch the Liebert EXM-2, here in Asia, where we are seeing strong demand for reliable power protection solution,” said Cheehoe Ling, vice president for infrastructure & solutions, Vertiv Asia and India.

Learn more on how to scale with confidence with Vertiv at www.Vertiv.com/SWC-Asia.

About Vertiv

Vertiv (NYSE: VRT) brings together hardware, software, analytics and ongoing services to ensure its customers’ vital applications run continuously, perform optimally and grow with their business needs.  Vertiv solves the most important challenges facing today’s data centers, communication networks and commercial and industrial facilities with a portfolio of power, cooling and IT infrastructure solutions and services that extends from the cloud to the edge of the network. Headquartered in Columbus, Ohio, USA, Vertiv employs approximately 20,000 people and does business in more than 130 countries. For more information, and for the latest news and content from Vertiv, visit Vertiv.com.

 

CONTACT

Katrina Tirante
T +6326203600 Ext 7666
E Katrina.Tirante@vertiv.com

Reinier Dungca
T +6326203600 Ext 7657
E Reinier.Dungca@vertiv.com

PORTALS
Overview
Partner Login

Language & Location