Sorry, this page isn't available for your location.

The page you're viewing is for Portuguese (EMEA) region.

Trabalhar com um representante do fabricante Vertiv permite que os designs complexos sejam configurados de acordo com as suas necessidades únicas. Se for uma organização que procura orientação técnica num projeto de grandes dimensões, a Vertiv pode fornecer o apoio de que necessita.

Saiba mais

Muitos clientes trabalham com um parceiro revendedor Vertiv, para comprar produtos Vertiv para as suas aplicações de IT. Os parceiros têm uma vasta formação e experiência, e estão posicionados de forma única para especificar, vender e apoiar soluções completas de TI e infraestruturas com produtos Vertiv.

Encontrar um revendedor

Já sabe do que precisa? Quer a conveniência da compra e do envio online? Determinadas categorias de produtos Vertiv podem ser adquiridas através de um revendedor online.


Encontre um revendedor on-line

Precisa de ajuda para escolher um produto? Fale com um Especialista Vertiv altamente qualificado que o ajudará a orientar-se para a solução certa para si.



Contacte um Especialista Vertiv

Sorry, this page isn't available for your location.

The page you're viewing is for Portuguese (EMEA) region.

E.ON and Vertiv Enter into Partnership for Critical Energy Infrastructures

junho 20, 2018

• Customers modernise energy systems and participate in the electricity market
• Changeover from lead to lithium batteries

Munich, Germany [June 20, 2018] – Energy company E.ON and technology provider Vertiv are combining their know-how in the field of energy solutions for critical infrastructures. This gives customers from trade and industry the opportunity to modernise their energy infrastructure in such a way that they can generate additional revenues on the energy market in addition to securing self-sufficiency. The solution, which is based on battery systems, will be offered on the German market as a first step.

In concrete terms, batteries ensure uninterruptible power supply in critical areas such as data centres, communication networks or industrial processes. With the E.ON and Vertiv concept, the battery not only functions as a back-up, but can also feed electricity in the other direction, i.e. into the public power grid, in times of low consumption or high own generation. The company then participates in the balancing energy market, capitalises on flexibility there, opens up a new source of income and stabilises the electricity grid at the same time.

Vertiv develops and installs the technical infrastructure for this complex solution, while E.ON is the interface to the energy market. The battery system will become part of E.ON's virtual power plant. The energy company aggregates the various producers and consumers and markets them. Commercial and industrial customers thus receive a guaranteed profit.

Lead-acid batteries are often used in critical energy infrastructures today. In the course of modernisation, the partners recommend the use of lithium batteries. They are smaller, lighter and have a larger number of charge-discharge cycles. In addition to a longer service life, lithium batteries also achieve a higher energy density and operate in a wider temperature range. Lithium batteries are therefore ideally suited for use in the energy market.

Bernd Schumacher, CEO of E.ON Connecting Energies, comments: “Our energy world is becoming increasingly decentralised. With the joint offer from E.ON and Vertiv, we are preparing our customers for this change. Your plants make a contribution to the energy transition, from which they even benefit. This economic and equally sustainable approach is a win-win situation.”

Reinhard Purzer, managing director of Vertiv in Germany, says: “Many of our UPS customers will certainly like to hear that they can now use their battery-based UPS systems profitably beyond their actual purpose. Our partnership with E.ON enables us to offer our customers this opportunity in a simple manner. In return, customers of E.ON who do not yet own a UPS system suitable for participation in the balancing energy market can conveniently use our joint offer. A great opportunity for all concerned!”

E.ON and Vertiv will present the new solution at the “The Smarter E Europe” trade show in Munich, Germany from June 20 to 22.

About Vertiv
Vertiv designs, builds and services critical infrastructure that enables vital applications for data centres, communication networks and commercial and industrial facilities. Formerly Emerson Network Power, Vertiv supports today’s growing mobile and cloud computing markets with a portfolio of power, thermal and infrastructure management solutions including the Chloride®, Liebert®, NetSure™ and Trellis™ brands. For more information, visit VertivCo.com.

Media Contact
Christine Wildgruber/Anna Erhardt
T +49 (0)89 / 41 95 99 27/-65/
E vertiv@maisberger.com

Acesso de Partner

Idioma e Localização