The page you're viewing is for Korean (Korea) region.

Vertiv 영업담당자에게 문의하시면 고객의 고유한 요구에 맞게 복잡한 설계를 구성할 수 있습니다. Vertiv는 대규모 프로젝트에 대한 기술 지침이 필요한 조직에 필요한 지원을 제공할 수 있습니다.

자세히 보기

많은 고객이 Vertiv 리셀러 파트너와 협력하여 IT 애플리케이션을 위한 Vertiv 제품을 구매합니다. 파트너는 다양한 교육을 받고 전문 경험을 보유하고 있으며 Vertiv 제품을 통해 전체 IT 및 인프라 솔루션을 지정, 판매, 지원할 수 있는 독보적인 위치에 있습니다.
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
Advanced thermal
management technologies

Addressing rapid evolution in the industry with emerging high density solutions

Addressing the challenges of the AI revolution​

Unlock unprecedented efficiency and thermal performance with two-phase direct-to-chip cooling solutions

High efficiency

DTC two-phase cooling enables more efficient heat transfer from the server components as the refrigerant changes phases from a liquid to a vapor at chip’s cold plate

Increase capacity

DTC two-phase cooling delivers higher cooling capacity per rack than traditional methods due to the phase change and increased heat capture properties of refrigerant

Reduced risks

DTC two-phase cooling uses refrigerant to remove heat from the chip. In the event of a system leak, the refrigerant evaporates, causing no damage
to the IT

Lower volume

The total volume of fluid and the flow rate required is much lower. This puts significantly less strain on the system and its components over time

The growing need for technological advancements​

Increased power densities of GPUs, CPUs and other components within a server and overall power consumption of IT equipment are driving dynamic discussion in the data center industry on what liquid cooling technologies will be required in the future. New generations of chips are packing other sub-systems into the IT equipment, such as memory and communication, which may require lower case temperatures than their processing counterparts.​

Liquid cooling solutions will not only need to meet thermal performance requirements of IT loads but also energy efficiencies of the overall data center. Vertiv, in collaboration with industry partners, is conducting studies on emerging liquid cooling technologies to increase technology and commercial readiness levels in an effort to be ready for mass deployments when the time comes in the industry. These include direct-to-chip two-phase, immersion cooling, and hybrid cooling technologies, each coming with their own benefits and challenges to consider.​

The growing need for technological advancements​

Increased power densities of GPUs, CPUs and other components within a server and overall power consumption of IT equipment are driving dynamic discussion in the data center industry on what liquid cooling technologies will be required in the future. New generations of chips are packing other sub-systems into the IT equipment, such as memory and communication, which may require lower case temperatures than their processing counterparts.​

Liquid cooling solutions will not only need to meet thermal performance requirements of IT loads but also energy efficiencies of the overall data center. Vertiv, in collaboration with industry partners, is conducting studies on emerging liquid cooling technologies to increase technology and commercial readiness levels in an effort to be ready for mass deployments when the time comes in the industry. These include direct-to-chip two-phase, immersion cooling, and hybrid cooling technologies, each coming with their own benefits and challenges to consider.​

Explore these emerging technologies

Enable exceptional scale, velocity, and quality for every project regardless of size or complexity.

Single-phase

  Direct-to-chip Immersion
Adoption Industry-adopted solution in fast-scaling stage Limited adoption due to accelerated computing trends and maintenance challenges​
Coolant Water or Water/Glycol​ Dielectric fluid​
Efficiency Depends on secondary water temperature design​ High
xPU Heat Flux < 300W/cm^2​ < 100W/cm^2​

Learn more about single-phase
direct-to-chip cooling

Two-phase

  Direct-to-chip Immersion
Adoption Increased adoption and aligned with future xPU roadmaps​ Very limited adoption due to design complexity and dielectric fluid regulations​
Coolant Boiling delectric fluid​ Boiling dielectric fluid​
Efficiency Very high due to use of higher facility water temperatures​ Very high​
xPU Heat Flux > 300W/cm^2​ < 300W/cm^2​​

Learn more about two-phase
direct-to-chip cooling

Single-phase

  Direct-to-chip Immersion
Adoption Industry-adopted solution Limited adoption
Coolant Industry-adopted solution Limited adoption
Efficiency Industry-adopted solution Limited adoption
xPU Heat Flux Industry-adopted solution Limited adoption

Learn more about single-phase
direct-to-chip cooling

Two-phase

  Direct-to-chip Immersion
Adoption Industry-adopted solution Limited adoption
Coolant Industry-adopted solution Limited adoption
Efficiency Industry-adopted solution Limited adoption
xPU Heat Flux Industry-adopted solution Limited adoption

Learn more about two-phase
direct-to-chip cooling

Custom Carousel with Two Tables

schematic diagram of single-phase direct-to-chip/cold plate cooling

How does single-phase direct-to-chip cooling work?​

Cold plates sit atop the heat-generating components (usually chips such as CPUs and GPUs) to draw off heat. Fluid flows through manifolds and in pipes through IT equipment, exchanging heat with cold plates to draw off heat without touching the chips. Air cooling is still required to extract heat from components that do not have a cold plate.

schematic diagram of single-phase direct-to-chip/cold plate cooling

How does two-phase direct-to-chip cooling work?​

Heat is generated in the silicon chip and captured at cold plates. That heat is then transferred to the refrigerant, which evaporates into a gaseous state. Via secondary fluid networks (SFNs), the vapor refrigerant moves to coolant distribution units (CDU) within the data center. These CDUs exchange the heat from the refrigerant to the primary (facility) loop for heat reuse or rejection, condensing the vapor refrigerant back into a liquid state. This primary fluid source can be water, water/glycol, or refrigerant based. The now liquid refrigerant is pumped back to the cold plates for another heat capture cycle.​

News release

Vertiv Collaborates with Intel on Liquid Cooled Solution for the Intel® Gaudi®3 AI Accelerator Platform

Boost AI performance and efficiency with two-phase direct-to-chip cooling

Read more

Get the right solution for the challenge​

Enable exceptional scale, velocity, and quality for every project regardless of size or complexity.

 
Cooling solutions CoolChip CDU XDRL​ CoolChip CDU XDRL rack​
Coolant distribution architecture​ Refrigerant to liquid​ Refrigerant to liquid​
Deployment type Row-based​​ Row-based​​
Total capacity Up to 500kW​​ Up to 200kW​
Refrigerant type R515B​​​ R515B​​​

Looking for a cooling solution?

Please fill out the form and we will get back to you as soon as possible

PORTALS
개요
파트너 로그인

언어 & 지역