The Vertiv™ Geist™ Rack Transfer Switch automatically switches to alternative power in less than 4 to 8 milliseconds
Mexico, DF [August 18, 2022] – Vertiv (NYSE: VRT), a global provider of critical digital infrastructure and continuity solutions, today introduced the Vertiv™ Geist™ Rack Transfer Switch (RTS), a new line of transfer switches that provides redundant power to single-corded devices. Available now throughout Latin America, North America and Asia, the Geist Rack Transfer Switch enables reliable switching to an alternative power source when the primary source fails or is unavailable. The space-saving device is ideal for use in distributed IT networks and edge locations.

Vertiv™ Geist™ Rack Transfer Switch (RTS)
The Vertiv Geist RTS instantly detects loss of power and automatically switches the load to an alternative source in less than 4 to 8 milliseconds, allowing the supported servers and other critical devices to continue to operate through a planned or unplanned outage. It is currently available in basic upgradeable and enhanced intelligence models, with switched and outlet-level monitored models launching later in 2022. Basic upgradeable models include the intelligence needed today, with the option to upgrade technology as needs evolve. Enhanced intelligence models provide a comprehensive view of critical IT equipment power usage, available either at the rack or via remote access.
The Geist RTS is available in 1U and 2U rack mount designs, enabling users to easily mount rack power distribution units (rPDUs) within the U-space of any standard rack or cabinet. Select models are available with Combination Outlet C13/C-19, simplifying the selection and purchasing process, and providing flexibility for customer applications.
“The need for compute is growing rapidly in Latin America and across the world”, said Rodrigo López, integrated rack systems offering manager at Vertiv LATAM. “The ability to provide dual power sources to single source data center equipment adds an extra level of availability and protection”.
In addition to providing redundant power, the Vertiv™ Geist™ RTS also proactively monitors the IT environment, including temperature, humidity, and airflow. Users also have the option to enhance device monitoring features, with remote monitoring of IT power usage. The Vertiv Geist RTS can support up to 24 outlets for higher-density rack configurations.
The Vertiv Geist RTS is ideal for banking, healthcare, financial services, education, energy, government and transportation industries that operate micro data centers, distributed IT networks or edge data centers.
For more information about the Vertiv™ Geist™ Rack Transfer Switch (RTS), and Vertiv’s products, visit Vertiv.com.
About Vertiv
Vertiv (NYSE: VRT) brings together hardware, software, analytics and ongoing services to enable its customers’ vital applications to run continuously, perform optimally and grow with their business needs. Vertiv solves the most important challenges facing today’s data centers, communication networks and commercial and industrial facilities with a portfolio of power, cooling and IT infrastructure solutions and services that extends from the cloud to the edge of the network. Headquartered in Columbus, Ohio, USA, Vertiv employs approximately 24,000 people and does business in more than 130 countries. For more information, and for the latest news and content from Vertiv, visit Vertiv.com.
Forward-Looking Statements
This release contains forward-looking statements within the meaning of the Private Securities Litigation Reform Act of 1995, Section 27 of the Securities Act, and Section 21E of the Securities Exchange Act. These statements are only a prediction. Actual events or results may differ materially from those in the forward-looking statements set forth herein. Readers are referred to Vertiv’s filings with the Securities and Exchange Commission, including its most recent Annual Report on Form 10-K and any subsequent Quarterly Reports on Form 10-Q for a discussion of these and other important risk factors concerning Vertiv and its operations. Vertiv is under no obligation to, and expressly disclaims any obligation to, update or alter its forward-looking statements, whether as a result of new information, future events or otherwise.
CONTACT
Ivis Fernandez
E ivis@ivicomm.com
P 3053355883