The page you're viewing is for English (LATAM) region.

Working with our Vertiv Sales team enables complex designs to be configured to your unique needs. If you are an organization seeking technical guidance on a large project, Vertiv can provide the support you require.

Learn More

Many customers work with a Vertiv reseller partner to buy Vertiv products for their IT applications. Partners have extensive training and experience, and are uniquely positioned to specify, sell and support entire IT and infrastructure solutions with Vertiv products.

Find a Reseller

Already know what you need? Want the convenience of online purchase and shipping? Certain categories of Vertiv products can be purchased through an online reseller.


Find an Online Reseller

Need help choosing a product? Speak with a highly qualified Vertiv Specialist who will help guide you to the solution that is right for you.



Contact a Vertiv Specialist

The page you're viewing is for English (LATAM) region.

Essential UPS Elements to Understand and How to Choose One that’s Best for your Business

In this age of digital transformation, when you’re increasingly relying on IT systems and data to keep your business running at peak efficiency, it’s more important than ever to ensure those systems can function even in the face of power disruptions.

That’s what uninterruptible power supplies (UPSs) are all about: supplying clean backup power to IT and other critical systems. In the face of a power disruption, a quality UPS can mean the difference between business as usual and lost data and hours of lost productivity.

UPSs can provide anywhere from a few minutes of backup power – enough to safely shut down workstations and servers or allow backup generators to kick in – up to several hours for certain equipment. Understanding how to choose a UPS that’s the best fit for your organization requires having a firm handle on how much power your IT and other critical systems draw and your tolerance for downtime for each application.

In this UPS buying guide, we’ll walk you through the UPS essentials and the buying criteria you need to consider to make an informed decision for your organization.

An uninterruptible power supply (UPS) provides clean, safe backup power for the attached electronic equipment. UPSs have internal batteries that are constantly being charged when not in use, so they’re ready to supply backup power in the event of a utility power outage or disruption. Additionally, UPSs can detect and compensate for anomalies such as power sags and surges, which are temporary power fluctuations that can damage attached computers and other electronics.

Different UPS models are designed to protect devices, including computers and peripherals, servers, and networking equipment, as well as data centers.

The best UPS battery backup solution for your organization depends on your specific requirements in terms of the loads you need to protect and tolerance for the risk of downtime.

While the cost of downtime varies widely by industry, 86% of respondents to a 2019 Statista survey put the cost at $301,000 per hour or more, and more than a third (34%) said downtime cost them $1 million per hour or more.

From that perspective, a relatively modest investment in a UPS is like an insurance policy against far more costly downtime and data loss.

UPSs protect against downtime caused by various kinds of power disruptions, including:

  • Power surges: Surges are short bursts of power that can result from a number of external and internal sources:
    • External: Utility maintenance work, lightning strikes, and power line disruptions, such as from snowstorms, downed tree limbs and transformer problems
    • Internal: Routine on/off cycling of motors in machinery, air conditioning and refrigeration units and more, as well as faulty wiring
  • Brownouts: which are reductions in the flow of utility power during high-demand periods
  • Unplanned power outages can result from issues including:
    • Lightning
    • Natural Disasters: hurricanes, snowstorms, high-speed winds, and other weather conditions
    • Utility and construction work
    • Motor Vehicle Accidents
  • Planned power outages:
    • Utility maintenance and system upgrades
    • Planned outages are now occurring in areas such as California, to protect against wildfires caused by sparks coming from utility equipment.

Buying the Right UPS: Key Considerations

Assessing which UPS battery backup is best for your business requires going through a series of questions regarding what equipment you need to protect, the ramifications of downtime with that equipment, whether a generator is available as a backup power source, and more.

  

1. Determine the size of the load that needs UPS protection, and, hence, the capacity of the UPS

Step one is assessing which IT or electronic devices warrant UPS battery backup protection and the power required by each device so that you can calculate the required UPS capacity. The power consumption of IT servers, computers and workstations, and networking equipment are obvious places to start. Still, you might also want to include other devices that are critical to the day-to-day operation of the business, e.g., point of sale equipment and security systems, among others. Assess what applications each component supports and how the loss of that application will affect your organization.

For each device to be connected to the UPS, determine the power consumption (watts) of that device.  Power consumption can typically be obtained from the equipment nameplate or manufacturer documentation.

The required UPS capacity is the sum of the power consumption of the devices to be connected to the UPS.
 

2. Assess the required UPS runtime for critical devices and applications

Step 2 is to determine the desired UPS runtime for continued operation in case of a power failure.

If you have a generator for extended backup power, the required runtime of the UPS may only be a few minutes (~5 minutes) to safely start-up and transition to the generator.

On the other hand, your primary goal may be to have enough runtime (~5 to 10 minutes) to safely shutdown servers and workstations to avoid any data loss or corruption.

Or, for some applications, such as networks and Internet access (very critical these days), you may want to have 1 to 2 hours of runtime to be able to ride through most outages.

Keep in mind that, in general, the more equipment you connect to a single UPS, the shorter its overall runtime will be.  An alternative may be to use separate UPS’ for certain applications.
 

3. Determine the number of outlets required

Add up the number of devices that you need the UPS to support, and make sure the UPS has enough outlets to meet your immediate needs, and also leave some room for growth.

Alternatively, you can use a power distribution unit (PDU) to provide additional outlets, but be careful not to overload the UPS.

Some UPS models also include outlets that only support surge protection.  These outlets do not provide battery backup. Make sure you understand the features of the UPS you are buying and that it has enough battery backup outlets to meet your needs.
 

4. Consider UPS installation requirements

UPSs come in a variety of sizes and form-factors. Tower models are standalone units that sit on the floor, or a desk or shelf, and often backup desktop computers, servers, and routers in an office environment.

Rack-mount UPS models are typically designed to fit in a standard 19-inch IT rack along with other IT equipment.  Rack-mount UPSs vary in size, and their height is measured by how many vertical slots it occupies in the rack. Each space is known as a “U” and measures 1.75 inches.

UPSs designed to use lithium-ion batteries tend to be smaller and lighter than similar models that use traditional lead-acid batteries, enabling you to fit more backup power capacity in the same space – or the same capacity in a smaller space.

UPS Advanced Features

UPSs can differ considerably in the exact set of features they support. The following are additional common features found in modern UPSs that you may want to consider.

 

Remote Monitoring and Management

UPSs with built-in network ports or support for network management cards (NMCs) can be monitored and managed remotely. This is especially important for UPSs installed in branch offices or edge locations with limited or no IT staff on site.  In this case, a centralized IT or facilities group can monitor the status of all UPSs and be notified of issues such as batteries that need replacement. NMCs may also support environmental sensors, enabling the remote monitoring of conditions such as temperature and humidity.
  

Remote UPS Outlet Control

Some UPS models include outlets or outlet groups that can be managed remotely, including the ability to monitor energy usage, and cycle power or turn off these outlets or outlet groups. This can enable someone in a remote operation center to reboot a hung server or network switch, for example.
  

LCD Control Panel

From a local perspective, an LCD screen on the UPS can display useful information such as battery health and power conditions, and facilitate local management and control of the UPS.
  

User Replaceable Batteries

No battery lasts forever, and UPS batteries are no exception. But given that the main purpose of a UPS is to ensure uptime, UPS battery replacement must be a quick and easy process.  Consider models that feature a removable panel that makes it easy for the user to replace the batteries, rather than having to call in a service technician.

Lithium-ion Batteries

Lithium-ion batteries are becoming more common in UPSs and for a good reason. They can easily last twice as long as traditional lead-acid batteries yet weigh far less and take up less space. They also support faster charging and more charge/discharge cycles. In many cases, the lower total cost of ownership (TCO) of a UPS with lithium-ion batteries will make them well worth the additional up-front cost. (To learn more, visit our Lithium-ion Batteries page.)
  

Extended Runtime

Some UPS models support external battery packs that can provide extended runtime beyond what a UPS’s internal battery offers, enabling users to get potentially hours of battery backup time for critical loads.
  

ECO-mode for Energy Savings

UPS Eco-mode seeks to save energy by bypassing the voltage regulation and/or energy conversion processes of the UPS if it determines that the utility input power is of good quality, to save energy.

 

We hope this UPS buying guide has helped you understand how to choose a UPS that will serve you well for the long-term. To learn more about choosing the best UPS battery backup solution for your organization, visit https://www.vertiv.com/en-latam/products-catalog/critical-power/uninterruptible-power-supplies-ups/.

PARTNERS
Partner Login

Language & Location