The page you're viewing is for English (LATAM) region.

Working with our Vertiv Sales team enables complex designs to be configured to your unique needs. If you are an organization seeking technical guidance on a large project, Vertiv can provide the support you require.

Learn More

Many customers work with a Vertiv reseller partner to buy Vertiv products for their IT applications. Partners have extensive training and experience, and are uniquely positioned to specify, sell and support entire IT and infrastructure solutions with Vertiv products.

Find a Reseller

Already know what you need? Want the convenience of online purchase and shipping? Certain categories of Vertiv products can be purchased through an online reseller.


Find an Online Reseller

Need help choosing a product? Speak with a highly qualified Vertiv Specialist who will help guide you to the solution that is right for you.



Contact a Vertiv Specialist

The page you're viewing is for English (LATAM) region.

Vertiv adds new single-phase, mixed voltage output ups models to fast-growing lithium-ion portfolio

30/10/24

Vertiv™ Liebert® GXT5 Lithium-Ion UPS family expands to include 5kVA to 10kVA Global Voltage (GV) models for critical edge deployments in Latin America

BOGOTA, Colombia [October 29, 2024] – Vertiv (NYSE: VRT), a global provider of critical digital infrastructure and continuity solutions, today introduced the extension of the Vertiv™ Liebert® GXT5 Lithium-Ion double-conversion, on-line uninterruptible power supply (UPS) system for 5kVA-10kVA Global Voltage (GV) (200V-240V) applications that meet the requirements of Latin American customers. The GV models are in addition to 1-3kVA Liebert® GXT 5 Lithium-Ion models, and further rounds out the Vertiv portfolio of lithium-ion UPS systems and solutions for the edge of the network. Vertiv is now accepting orders for the new Liebert GXT5 Lithium Ion, 5-10kVA GV models in Latin America. 

The Liebert GXT5 Lithium-Ion models are designed for the smaller spaces typical of the network edge, with a convertible rack/tower design and only a 3U (5kVA to 10kVA UPS) rack height. The new GV models include an integrated maintenance bypass cabinet, preserving additional rack U-space. All Liebert GXT5 Lithium-Ion UPS systems come with a five-year limited warranty.  

The higher power density of lithium-ion batteries enabled Vertiv to pack more runtime in less space compared to a typical UPS with valve-regulated lead acid (VRLA) batteries, and that runtime can be extended with up to eight external battery cabinets. The batteries allow higher operating temperatures and longer life expectancy and can reduce the total cost of ownership by up to 50% compared to VRLA solutions. In addition, lithium-ion batteries typically last eight to 10 years, compared to about three to five years for VRLA batteries, reducing or eliminating the cost and inconvenience of battery replacements during the life of the UPS.

”The new Liebert GXT5 Lithium-Ion GV brings to Latin America an ideal solution for more demanding environments in terms of operating temperature, extended lifespan, and backup time within the single-phase UPS segment, providing significant benefits in operation and infrastructure replacement cycles. This is especially valued by users with a large number of distributed sites with varied voltages across cities and/or countries,” stated David Goncalvez, offering and strategy manager for Vertiv, LATAM.

According to Omdia’s report, Market Landscape: Battery Energy Storage Systems, lithium-based battery adoption for UPS in data centers is expected to continue its fast growth and soon dominate the UPS battery market, reaching 65% of global revenue by 2030. 

For more information on the Vertiv™ Liebert® GXT5 Lithium-Ion UPS family or other Vertiv power and cooling solutions, visit Vertiv.com.

About Vertiv

Vertiv (NYSE: VRT) brings together hardware, software, analytics and ongoing services to enable its customers’ vital applications to run continuously, perform optimally and grow with their business needs. Vertiv solves the most important challenges facing today’s data centers, communication networks and commercial and industrial facilities with a portfolio of power, cooling and IT infrastructure solutions and services that extends from the cloud to the edge of the network. Headquartered in Columbus, Ohio, USA, Vertiv does business in more than 130 countries. For more information, and for the latest news and content from Vertiv, visit Vertiv.com. 

Forward-Looking Statements

This release contains forward-looking statements within the meaning of the Private Securities Litigation Reform Act of 1995, Section 27 of the Securities Act, and Section 21E of the Securities Exchange Act. These statements are only a prediction. Actual events or results may differ materially from those in the forward-looking statement set forth herein. Readers are referred to Vertiv’s filings with the Securities and Exchange Commission, including its most recent Annual Report on Form 10-K and any subsequent Quarterly Reports on Form 10-Q for a discussion of these and other important risk factors concerning Vertiv and its operations. Vertiv is under no obligation to, and expressly disclaims any obligation to, update or alter its forward-looking statements, whether as a result of new information, future events or otherwise. 

MEDIA CONTACT

Angélica Molinas

Latam Marketing Communications Manager

E: Angelica.Molinas@vertiv.com

  

Partner Login

Language & Location