Vertiv™ SmartAisle™ 3 combines power, thermal management, monitoring and power distribution to support digital environments with increasing capacity requirements
Brazil, [September XX, 2026] – Vertiv (NYSE: VRT), a global leader in critical digital infrastructure, today announced the launch of Vertiv™ SmartAisle™ 3, a modular data center solution that integrates power backup, thermal management, monitoring and power distribution within a single architecture. Available in Argentina, Chile, Peru, Uruguay, Paraguay, Brazil and Bolivia, the solution can be configured to support up to 120 kW of total IT load.
Vertiv SmartAisle 3 combines racks, uninterruptible power supply (UPS), thermal management, monitoring and physical security within an integrated solution. Its architecture incorporates artificial intelligence and self-learning capabilities designed to support system operation and energy management.
Among these capabilities, the solution can monitor operating conditions and adjust temperature according to the environment. These features can help achieve energy savings of up to 20% compared with systems without AI functionality, while maintaining the defined operating conditions for the infrastructure.
“Data-intensive applications are leading more organizations to evaluate how they can expand or modernize their infrastructure without adding unnecessary operational complexity,” said Felipe Vasco, Technology Applications Director for Vertiv LATAM. “Vertiv SmartAisle 3 brings together power, thermal management, distribution and monitoring within a modular architecture that can adapt to different capacity and deployment requirements, while incorporating monitoring and control capabilities that support infrastructure operations.”“Vertiv SmartAisle 3 brings together power, thermal management, distribution and monitoring within a modular architecture that can adapt to different capacity and deployment requirements, while incorporating monitoring and control capabilities that support infrastructure operations.”
The solution includes a flexible busway power distribution system designed to simplify power distribution within the modular environment and reduce the complexity associated with onsite cabling. It also incorporates integrated cabling, front and rear rack sensors and centralized monitoring capabilities to supervise variables such as temperature, humidity and door status.
Vertiv SmartAisle 3 also includes a 15-inch touchscreen control panel and the option to upgrade to a 95-inch local door display, providing greater visibility into operating conditions and supporting system monitoring and troubleshooting.Vertiv SmartAisle 3 also includes a 15-inch touchscreen control panel and the option to upgrade to a 95-inch local door display, providing greater visibility into operating conditions and supporting system monitoring and troubleshooting.
The solution can simplify the management of monitoring and environmental control systems, helping reduce the operational failure cycle by up to 75%. In addition, by integrating and testing key components at the factory before onsite installation.
Vertiv™ SmartAisle™ 3 is part of Vertiv’s portfolio of integrated modular solutions and can support a range of applications across sectors including banking and financial services, government, education, edge infrastructure and other environments that require power, cooling and monitoring to be integrated within a modular solution.
For more information about Vertiv SmartAisle 3 and Vertiv integrated solutions, visit Vertiv.com.
About Vertiv
Vertiv (NYSE: VRT) brings together hardware, software, analytics and ongoing services to enable its customers’ vital applications to run continuously, perform optimally and grow with their business needs. Vertiv solves the most important challenges facing today’s data centers, communication networks and commercial and industrial facilities with a portfolio of power, cooling and IT infrastructure solutions and services that extends from the cloud to the edge of the network. Headquartered in Westerville, Ohio, USA, Vertiv does business in more than 130 countries. For more information, and for the latest news and content from Vertiv, visit Vertiv.com.
Forward-looking statements
This release contains forward-looking statements within the meaning of the Private Securities Litigation Reform Act of 1995, Section 27 of the Securities Act, and Section 21E of the Securities Exchange Act. These statements are only a prediction. Actual events or results may differ materially from those in the forward-looking statements set forth herein. Readers are referred to Vertiv’s filings with the Securities and Exchange Commission, including its most recent Annual Report on Form 10-K and any subsequent Quarterly Reports on Form 10-Q for a discussion of these and other important risk factors concerning Vertiv and its operations. Vertiv is under no obligation to, and expressly disclaims any obligation to, update or alter its forward-looking statements, whether as a result of new information, future events or otherwise.
CONTACT
Pedro Pizarro
T +57 3202818429