Vertiv™ Liebert® PSI5 Lithium-Ion single-phase line targets manufacturing, education and edge applications needing long battery life
Mexico, DF [Dec. 8, 2021] – Vertiv (NYSE: VRT), a global provider of critical digital infrastructure and continuity solutions, today expanded its portfolio of uninterruptible power supply (UPS) systems with lithium-ion battery options with Liebert® PSI5 Lithium-Ion line-interactive UPS family. Liebert PSI5 Lithium-Ion is available in 1500, 2200 and 3000VA models, including the industry’s first 1500VA lithium-ion line-interactive tower. Targeted for edge and distributed IT applications, the 120V Liebert PSI5 is available in Mexico, Colombia, Ecuador, Venezuela, Central America and the Caribbean through local Vertiv sales offices and value added resellers.
In comparison to valve-regulated lead acid (VRLA) batteries, lithium-ion batteries have up to 3x longer battery life, perform better at higher temperatures, are smaller, lighter and deliver longer runtimes. The Liebert PSI5 Lithium-Ion family will provide approximately 7-9 minutes of battery backup at full load compared to an estimated 3-5 minutes for a standard UPS with VRLA batteries.
“The benefits of lithium-ion are undeniable and rapid market adoption has pushed prices down to the point that the total cost of ownership clearly favors lithium,” said Jeff Kessen, senior vice president for global product transformation at Vertiv. “We’ve seen adoption increase steadily in the data center, and as more lithium-ion UPS options become available for edge locations, that pattern is repeating.”
“As digitalization increases in Latin America, many applications are moving to the edge of the network and require reliable power protection,” said Guillermo Maddalena, power management and software solutions offering manager at Vertiv in Latin America. “UPS systems with lithium-ion batteries offer cost and operational benefits, by eliminating on-going site visits to replace failed batteries. Ultimately this means lower costs and higher system availability for critical edge deployments, and a wider range of options for our customers.”
The Liebert® PSI5 Lithium-Ion UPS comes with a five-year warranty on the electronics and battery. It is accompanied by a range of start-up and on-site service options.
For information on using lithium-ion batteries with single-phase UPS systems, download the Vertiv white paper, The Advantages of Using Lithium-Ion Batteries as A Backup Power Source in Single-Phase UPS Applications for Remote and Edge Data Centers.
For more information on the Liebert PSI5 Lithium-Ion and other UPS systems from Vertiv, visit Vertiv.com or connect on social media: Facebook, LinkedIn, Instagram and Twitter.
About Vertiv
Vertiv (NYSE: VRT) brings together hardware, software, analytics and ongoing services to ensure its customers’ vital applications run continuously, perform optimally and grow with their business needs. Vertiv solves the most important challenges facing today’s data centers, communication networks and commercial and industrial facilities with a portfolio of power, cooling and IT infrastructure solutions and services that extends from the cloud to the edge of the network. Headquartered in Columbus, Ohio, USA, Vertiv employs approximately 21,000 people and does business in more than 130 countries. For more information, and for the latest news and content from Vertiv, visit Vertiv.com.
Forward-Looking Statements
This release contains forward-looking statements within the meaning of the Private Securities Litigation Reform Act of 1995, Section 27 of the Securities Act, and Section 21E of the Securities Exchange Act. These statements are only a prediction. Actual events or results may differ materially from those in the forward-looking statement set forth herein. Readers are referred to Vertiv’s filings with the Securities and Exchange Commission, including its most recent Annual Report on Form 10-K/A and any subsequent Quarterly Reports on Form 10-Q for a discussion of these and other important risk factors concerning Vertiv and its operations. Vertiv is under no obligation to, and expressly disclaims any obligation to, update or alter its forward-looking statements, whether as a result of new information, future events or otherwise.
CONTACT
Ivis Cruz Fernandez
icruz@fusioncomminc.com