Vertiv and Febicom join forces to offer a complete data center solution for the wholesaler Nini in Buenos Aires.
Buenos Aires, [December 3, 2020] Vertiv (NYSE: VRT), a global provider of critical digital infrastructure and continuity solutions, is working alongside Febicom, an integrator specializing in information technology and infrastructure projects, to provide an integrated solution for the complete assembly of a data center for Nini, a wholesale shopping center. The solution includes a modular uninterruptible power supply (UPS) system and precision cooling to safeguard operational continuity.
The project consisted of the integrated construction of a data center from the ground up, including the electrical installation, as well as the incorporation of a computing, printing, and storage system. The infrastructure also had to have redundancy in the electrical system built in, so that the solutions could remain in operation until the generator was turned on, ensuring business continuity in the event of failures in the electricity supply.
“We are proud to be working with an integrator like Febicom, whose experience and dedication allows us to add value for important clients such as Nini, so that their digital systems will remain available and goods can be efficiently supplied to over 3,000 stores in the Buenos Aires area,” says Mariana Coste, Vertiv’s channel manager for the region of Argentina, Paraguay, Uruguay and Bolivia.
Three Liebert® CRV 035 35kW precision row-based direct expansion air conditioning systems were installed, along with a 150 kW Liebert® APM transformer-free UPS system with battery backup and redundant power modules in an N+1 configuration, along with a monitoring system based on SNMP protocols for cooling equipment as well as for modular UPS.
“Since this was a large depot, power continuity was one of our priorities,” says Daniel Felicitato, General Manager of Febicom. “Constant contact with Vertiv’s engineers, who advised and worked alongside us throughout the process from end to end, was vital to achieving a successful implementation that guaranteed the client’s objectives.”
As a result of this implementation, Nini’s data center employs hot and cold aisle containment to optimize efficiency. All industry best practices have been applied in its construction and design in order to support a major logistics operation with 1,100 pallets coming in on a normal day, with 127,000 boxes and 194,000 individual items selected.
“This implementation is very important as it confirms our expertise as continuity architects who collaborate with our clients to help them build their digital infrastructures and intelligent ecosystems, for uninterrupted, secure and reliable digital operations,” concluded Mariana Coste.
For more information about Vertiv, visit Vertiv.com or on social media: Facebook, LinkedIn, and Twitter.
About Vertiv
Vertiv (NYSE: VRT) brings together hardware, software, analytics and ongoing services to ensure its customers’ vital applications run continuously, perform optimally and grow with their business needs. As Architects of Continuity™, Vertiv solves the most important challenges facing today’s data centers, communication networks and commercial and industrial facilities with a portfolio of power, cooling and IT infrastructure solutions and services that extends from the cloud to the edge of the network. Headquartered in Columbus, Ohio, USA, Vertiv employs approximately 20,000 people and does business in more than 130 countries. For more information, and for the latest news and content from Vertiv, visit Vertiv.com.
About Fabicom
We are a company that has specialized in providing integrated information technology solutions, systems, communications and computer projects since 1992. Our objective is to provide our clients with a suitable solution for every case by undertaking a functional analysis of their needs that begins with consulting and continues with engineering services, design and analysis, and finally implementation, commissioning and subsequent maintenance, thus ensuring the best technological solution. We have a staff of highly trained professionals with extensive field experience, which allows us to gain the trust of our customers as we implement new projects and provide support to their operations in critical situations. Our greatest asset is our customers’ trust and satisfaction. That is our commitment.
CONTACT
Bárbara Keilty
P 005491157107143
E barbara@brand-partners.com.ar