The page you're viewing is for English (India) region.

Working with our Vertiv Sales team enables complex designs to be configured to your unique needs. If you are an organization seeking technical guidance on a large project, Vertiv can provide the support you require.

Learn More

Many customers work with a Vertiv reseller partner to buy Vertiv products for their IT applications. Partners have extensive training and experience, and are uniquely positioned to specify, sell and support entire IT and infrastructure solutions with Vertiv products.

Find a Reseller

Already know what you need? Want the convenience of online purchase and shipping? Certain categories of Vertiv products can be purchased through an online reseller.


Find an Online Reseller

Need help choosing a product? Speak with a highly qualified Vertiv Specialist who will help guide you to the solution that is right for you.



Contact a Vertiv Specialist

The page you're viewing is for English (India) region.

Vertiv announces scalable, high-capacity double stack busway system that preserves white space for growing AI data center demands

3-3-26

The Vertiv™ PowerBar Track double stack configuration delivers flexible overhead power distribution for modern compute environments

COLUMBUS, Ohio [March 3, 2025] – Vertiv (NYSE: VRT), a global leader in critical digital infrastructure, today announced the expansion of the Vertiv™ PowerBar Track busway family with the introduction of a compact, high-capacity double-stack design that enables higher power density while optimizing valuable white-space. Designed to address rapidly evolving AI workloads within colocation and hyperscale data centers, the scalable system delivers high-capacity power distribution through a flexible, modular architecture that supports future growth, enables improved energy efficiency, and provides simplified deployment. The solution is designed to meet rigorous global safety and performance standards, with configurations of up to 2000A under UL standard 857, and up to 2500A for IEC 61439-6 with variants in copper and aluminum conductors.

The Vertiv PowerBar Track enables safe, continuous power delivery and live configuration changes without system downtime. Its open-track architecture allows operators to install or relocate tap-off boxes anywhere along the busway while maintaining active load distribution. Each connection point includes built-in mechanical and electrical interlocks for operator safety, and optional integrated metering provides real-time visibility of power usage for improved capacity planning and energy management. The double stack configuration supports higher capacity and more connections per tap-off box and can also scale vertically to efficiently serve high density environments.

“Power distribution must keep pace with the scale and density of modern AI and high-performance computing environments,” said Kyle Keeper, senior vice president of the power business unit at Vertiv. “As customers navigate increasing power demands, tighter space constraints, and rapidly evolving infrastructure requirements, they need solutions that provide flexibility. Vertiv PowerBar Track double stack is designed to address these challenges by enabling compact yet scalable expansion, supporting live changes, and delivering the reliability required in mission-critical data center environments.”

The busway system integrates seamlessly with the broader Vertiv end-to-end power train, including Vertiv™ PowerBoard switchgear, uninterruptible power supply (UPS) systems, and racks, forming a complete and coordinated infrastructure for high-density applications. Supported by Vertiv’s global manufacturing and service network, Vertiv™ PowerBar Track can be configured to aid maintenance, helping reduce maintenance-related downtime while enabling faster deployment and greater adaptability for data centers undergoing rapid expansion. Vertiv PowerBar Track also contributes to the Vertiv™ 360AI power ecosystem, which combines power distribution, protection, and management technologies designed to support the next generation of AI-ready digital infrastructure.

Vertiv PowerBar Track integrates with Vertiv™ OneCore, a scalable prefabricated data center infrastructure solution, and Vertiv™ SmartRun, a modular overhead IT infrastructure system, enabling a cohesive approach to modular, scalable data center design.

For more information about Vertiv PowerBar Track and Vertiv’s end-to-end power and thermal management solutions, visit Vertiv.com.

About Vertiv

Vertiv (NYSE: VRT) brings together hardware, software, analytics and ongoing services to enable its customers’ vital applications to run continuously, perform optimally and grow with their business needs. Vertiv solves the most important challenges facing today’s data centers, communication networks and commercial and industrial facilities with a portfolio of power, cooling and IT infrastructure solutions and services that extends from the cloud to the edge of the network. Headquartered in Westerville, Ohio, USA, Vertiv does business in more than 130 countries. For more information, and for the latest news and content from Vertiv, visit Vertiv.com.

Forward-looking statements

This release contains forward-looking statements within the meaning of the Private Securities Litigation Reform Act of 1995, Section 27 of the Securities Act, and Section 21E of the Securities Exchange Act. These statements are only a prediction. Actual events or results may differ materially from those in the forward-looking statements set forth herein. Readers are referred to Vertiv’s filings with the Securities and Exchange Commission, including its most recent Annual Report on Form 10-K and any subsequent Quarterly Reports on Form 10-Q for a discussion of these and other important risk factors concerning Vertiv and its operations. Vertiv is under no obligation to, and expressly disclaims any obligation  to, update or alter its forward-looking statements, whether as a result of new information, future events or otherwise.

CONTACT
Ruder Finn
E 
Vertiv@RuderFinn.com

PRODUCTS & SERVICES
Partner Login

Language & Location