The page you're viewing is for English (EMEA) region.

Working with our Vertiv Sales team enables complex designs to be configured to your unique needs. If you are an organization seeking technical guidance on a large project, Vertiv can provide the support you require.

Learn More

Many customers work with a Vertiv reseller partner to buy Vertiv products for their IT applications. Partners have extensive training and experience, and are uniquely positioned to specify, sell and support entire IT and infrastructure solutions with Vertiv products.

Find a Reseller

Already know what you need? Want the convenience of online purchase and shipping? Certain categories of Vertiv products can be purchased through an online reseller.


Find an Online Reseller

Need help choosing a product? Speak with a highly qualified Vertiv Specialist who will help guide you to the solution that is right for you.



Contact a Vertiv Specialist

The page you're viewing is for English (EMEA) region.

Vertiv Expands Rack PDU Portfolio for High-Density Computing Applications for AI and HPC Deployments in North America and EMEA

September 03, 2025

Vertiv™ PowerIT rack power distribution units (PDUs) are now available in power ratings up to 57.6 kW

LONDON, UK [September 3, 2025] – Vertiv (NYSE: VRT), a global leader in critical digital infrastructure, today announced the new Vertiv™ PowerIT rack power distribution units (PDU), an extension of the Vertiv PowerIT product line. These models are designed to address the rising power needs of data-intensive workloads, including AI and high-performance computing (HPC). They provide advanced power management, flexible configurations, and enhanced internal components for greater reliability, enabling data centres to seamlessly scale power in response to growing IT demands. Basic, monitored and switched models are available now in North America, Europe, the Middle East and Africa (EMEA).

With racks increasingly supporting power densities above 25 kW, data centre operators require robust high-capacity power distribution solutions capable of balancing loads and managing essential electrical requirements efficiently. Vertiv PowerIT rack PDU utilises three-phase power distribution in both 208V Delta (commonly used in North America) and 240/415V WYE configurations (typical in EMEA and other international markets), an approach that evenly distributes electrical load across multiple phases, reducing potential for circuit overload risks, stabilising voltage and enhancing reliability.

“The growing adoption of AI and HPC applications is driving unprecedented power demands in data centres. Vertiv™ PowerIT rack PDU demonstrates our commitment to meeting these evolving needs with an end-to-end portfolio" said Andrea Ferro, VP power & IT systems for Vertiv in EMEA. "By providing solutions specifically engineered for high-density computing, we're enabling our EMEA and global customers to efficiently scale their power infrastructure while maintaining the reliability and flexibility needed for next-generation data centres.”

Vertiv PowerIT rack PDU provides precise real-time power usage data to support optimised energy management in monitored and switched models. Built for rugged performance, the rack PDU reliably operates in temperatures up to 140°F (60°C) in environmental conditions up to 95% humidity, providing consistent performance and adaptability even in the most demanding, high-density data centre environments. Switched versions offer remote outlet-level control, rapid deployment adjustments and enhanced protection for critical IT loads. The monitored models have Secure Boot security feature, with a hardware trust anchor that is proprietary to Vertiv, that protects the integrity of the network card’s firmware by preventing unauthorised modifications. With configure-to-order and engineered-to-order options, customers can tailor the rack PDUs to their specific needs by selecting outlet configurations, input types and chassis colours.

Vertiv PowerIT rack PDU is available with the Vertiv™ Distribution Assurance Package, providing seven-year comprehensive coverage, 24/7 emergency response, on-site and remote support, and professional startup services to support ongoing reliability and maximise uptime.

For more information about the Vertiv PowerIT rack PDU or Vertiv’s full portfolio of end-to-end power management and thermal management solutions, visit Vertiv.com. To find the right rack PDU for your application, explore the Vertiv™ rPDU Finder.

About Vertiv

Vertiv (NYSE: VRT) brings together hardware, software, analytics and ongoing services to enable its customers’ vital applications to run continuously, perform optimally and grow with their business needs. Vertiv solves the most important challenges facing today’s data centres, communication networks and commercial and industrial facilities with a portfolio of power, cooling and IT infrastructure solutions and services that extends from the cloud to the edge of the network. Headquartered in Westerville, Ohio, USA, Vertiv does business in more than 130 countries. For more information, and for the latest news and content from Vertiv, visit Vertiv.com.

Forward-looking statements

This release contains forward-looking statements within the meaning of the Private Securities Litigation Reform Act of 1995, Section 27 of the Securities Act, and Section 21E of the Securities Exchange Act. These statements are only a prediction. Actual events or results may differ materially from those in the forward-looking statements set forth herein. Readers are referred to Vertiv’s filings with the Securities and Exchange Commission, including its most recent Annual Report on Form 10-K and any subsequent Quarterly Reports on Form 10-Q for a discussion of these and other important risk factors concerning Vertiv and its operations. Vertiv is under no obligation to, and expressly disclaims any obligation to, update or alter its forward-looking statements, whether as a result of new information, future events or otherwise.

CONTACT

E  susanna.collins@apodpr.co.uk

Related Articles

Partner Login

Language & Location