Vertiv™ PowerUPS 200 Series is a highly featured uninterruptible power supply system for multiple devices with enhanced protection from power loss and voltage instability now available in EMEA
London, UK [February 2, 2026] – Vertiv (NYSE: VRT), a global leader in critical digital infrastructure, today introduced a new generation of compact uninterruptible power supply (UPS) systems for connected homes and workspaces. The Vertiv™ PowerUPS 200 family, available in 600 to 2200 VA capacities, combines modern design with enhanced usability for workstations, point-of-sale (POS) systems, gaming consoles, smart devices, and home entertainment setups. Now available in Europe, the Middle East and Africa (EMEA), the series expands Vertiv’s single-phase UPS portfolio for home, office, and retail environments.
“As digital demand accelerates, users are increasingly looking for reliable power solutions, without operational complexity,” said Giuseppe Leto, senior director, IT Systems for Vertiv in EMEA. “The Vertiv PowerUPS 200 family combines solid engineering expertise with an intuitive design tailored for the modern spaces where people live and work today.”
Designed for ease of use and everyday reliability, the Vertiv™ PowerUPS 200 Standard Line Interactive Series (230V) and Vertiv™ PowerUPS 200 Essential Line Interactive Series (230 V) include practical benefits that make power protection simpler and more intuitive. Among the most notable features are user-replaceable batteries, which allow users to safely extend product life, and a straightforward interface featuring runtime LED indicators on Vertiv PowerUPS 200 Essential Line Interactive Series models, and a color LCD display on Vertiv PowerUPS 200 Standard Line Interactive Series models for clear system status visibility.
Models 1000VA and higher include Type-A and Type-C USB charging ports, providing convenient power for mobile and connected devices. The new design also integrates details such as a dedicated mute button for alarm management and recyclable packaging, complementing proven performance features including automatic voltage regulation (AVR) for stable output, and optimized internal design for consistent performance across a wide voltage range.
The Vertiv™ PowerUPS 200 Essential Line Interactive Series (230 V) and Vertiv™ PowerUPS 200 Standard Line Interactive Series (230 V) include models with up to eight total outlets, depending on configuration. Compact dimensions and recyclable packaging make them suitable for modern workspaces, while the two-year warranty (Essential Series) and the three-year warranty (Standard Series), including battery coverage, provides added confidence for users.
The Vertiv PowerUPS 200 Series renews Vertiv’s single-phase desktop portfolio, delivering reliable and efficient power protection for home, office, and small IT environments. Together with the network models such as Vertiv™ Edge Line-Interactive UPS and Vertiv™ Liebert® GXT5 UPS, the series is part of Vertiv’s comprehensive power management ecosystem, supporting future-ready digital operations.
For more information about the Vertiv PowerUPS 200 series, visit Vertiv.com.
About Vertiv
Vertiv (NYSE: VRT) brings together hardware, software, analytics and ongoing services to enable its customers’ vital applications to run continuously, perform optimally and grow with their business needs. Vertiv solves the most important challenges facing today’s data centers, communication networks and commercial and industrial facilities with a portfolio of power, cooling and IT infrastructure solutions and services that extends from the cloud to the edge of the network. Headquartered in Westerville, Ohio, USA, Vertiv does business in more than 130 countries. For more information, and for the latest news and content from Vertiv, visit Vertiv.com.
Forward-looking statements
This release contains forward-looking statements within the meaning of the Private Securities Litigation Reform Act of 1995, Section 27 of the Securities Act, and Section 21E of the Securities Exchange Act. These statements are only a prediction. Actual events or results may differ materially from those in the forward-looking statements set forth herein. Readers are referred to Vertiv’s filings with the Securities and Exchange Commission, including its most recent Annual Report on Form 10-K and any subsequent Quarterly Reports on Form 10-Q for a discussion of these and other important risk factors concerning Vertiv and its operations. Vertiv is under no obligation to, and expressly disclaims any obligation to, update or alter its forward-looking statements, whether as a result of new information, future events or otherwise.
CONTACT
Susanna Collins
E susanna.collins@apodpr.co.uk