Sorry, this page isn't available for your location.

The page you're viewing is for English (EMEA) region.

Working with our Vertiv Sales team enables complex designs to be configured to your unique needs. If you are an organization seeking technical guidance on a large project, Vertiv can provide the support you require.

Learn More

Many customers work with a Vertiv reseller partner to buy Vertiv products for their IT applications. Partners have extensive training and experience, and are uniquely positioned to specify, sell and support entire IT and infrastructure solutions with Vertiv products.

Find a Reseller

Already know what you need? Want the convenience of online purchase and shipping? Certain categories of Vertiv products can be purchased through an online reseller.


Find an Online Reseller

Need help choosing a product? Speak with a highly qualified Vertiv Specialist who will help guide you to the solution that is right for you.



Contact a Vertiv Specialist

Sorry, this page isn't available for your location.

The page you're viewing is for English (EMEA) region.

Static UPS: The Future-Proofed Choice for A Shifting Energy Landscape

December 13, 2018

The main role of any Uninterruptible Power Supply (UPS) is to ensure the availability of the critical infrastructure which it supports. Different UPS designs have emerged and the technology continues to be improved and developed.

This whitepaper examines how the static UPS, the dominant technology in most regions, compares with rotary designs when set against the backdrop of changing customer business demands, as well as evolving energy grid and environmental regulations.

Key Findings:

  • Static UPS technology is by far the most widely adopted type of large (> 500 kW) UPS technology (three-phase) because of its efficiency and flexibility
  • Static UPS also enables the modular configuration of a completely redundant power and control system, sized to match the capacity of the protected equipment
  • The design of rotary UPS means equipment is usually a more fixed investment than modular static technology and often needs to be oversized against possible future growth
  • Static UPS equipped with Lithium-Ion Batteries (LIB) have several advantages over conventional Valve-Regulated Lead-Acid (VRLA) batteries. They are 70% smaller and considerably lighter. LIB also support higher operating temperatures better than VRLA, which can also help cut battery cooling costs
  • As electricity grids evolve, the static UPS system can be a good fit for delivering emerging front-of-meter (FtM) and behind-the-meter (BtM) energy storage applications
  • Large rotary UPS are often installed before walls of the building are closed. The weight of rotary equipment requires a stronger building structure; there also could be very strict requirements because of the vibration caused by flywheels
  • Electronic equipment usually requires less maintenance on average than mechanical equipment. For example, a static UPS system often only requires a single maintenance inspection in a 12-month period
Download White Paper

Related Articles

PARTNERS
Overview
Consultants Corner
Partner Login

Language & Location