The page you're viewing is for English (Canada) region.

Working with our Vertiv Sales team enables complex designs to be configured to your unique needs. If you are an organization seeking technical guidance on a large project, Vertiv can provide the support you require.

Learn More

Many customers work with a Vertiv reseller partner to buy Vertiv products for their IT applications. Partners have extensive training and experience, and are uniquely positioned to specify, sell and support entire IT and infrastructure solutions with Vertiv products.

Find a Reseller

Already know what you need? Want the convenience of online purchase and shipping? Certain categories of Vertiv products can be purchased through an online reseller.


Find an Online Reseller

Need help choosing a product? Speak with a highly qualified Vertiv Specialist who will help guide you to the solution that is right for you.



Contact a Vertiv Specialist

The page you're viewing is for English (Canada) region.

cisco-logo-2022
Cisco Live 2022
June 12 - June 16, 2022
Mandalay Bay Convention Center, Las Vegas, Nevada,
800x400-nrf.jpg

Come meet the Vertiv team at Cisco Live 2022! Cisco Live delivers education and inspiration to technology innovators worldwide through large-scale in-person and digital events, as well as on-demand education. At Cisco Live, Vertiv’s team of experts will be discussing our solutions designed to help support the equipment needed to support our growing digital world.

Come see us in booth #3250 and see our latest solutions designed to keep your critical IT equipment protected and performing at its highest level. Products at this year’s booth include:

The Vertiv™ Avocent® ADX Ecosystem (ADX MP1000, ADX RM1048 and ADX IPUHD and IPIQ) securely and efficiently manages multiple devices, creating an enhanced user experience with its 4K over IP capability. Its secure common architecture seamlessly integrates and scales to create an open yet resilient IT management platform. The Avocent ADX Ecosystem can support 100+ simultaneous users, enabling automation, management, monitoring, and control of all of your devices easier than ever – all with the fastest and most feature-rich KVM experience on a single device.

The  Avocent® ACS8000 advanced console server series offers new connectivity features such as cellular, gigabit fiber, USB and sensors. IT professionals and network operations center (NOC) personnel can now harness these new capabilities to further enable them to perform secure, remote data center management and out-of-band management of IT assets from anywhere in the world.

Vertiv™ Environet™ Alert provide businesses with critical facility monitoring software that is affordable and easy to use. This solution delivers superior monitoring, alerting, trending and data organization capabilities to help companies protect and grow their business.

Network switches, load balancers and routers typically sit at the top and back portion of the rack, away from the cold aisle airflow at the front of the cabinet, increasing the chance of failure over time. The Vertiv™ Geist™ SwitchAir® helps prevent failure by channeling cool air from the front of the rack to the air intakes regardless of where the equipment is mounted.

The new Vertiv™ Geist™ Rack Transfer Switch delivers redundant power to single corded devices when it automatically detects the loss of power and switches the power load to the alternative power source in less than 4-8 milliseconds. This ensures equipment remains powered until the primary power source returns providing ultimate mission-critical power reliability.

The Vertiv™ Geist™ UPDU is a versatile rack power distribution unit that supports common AC power configurations ranging from 16A-60A and 120V-415V. The universal design simplifies critical IT infrastructure deployments by allowing a single model to be installed globally.

The Vertiv™ Liebert® GXT5 Lithium-Ion double-conversion online UPS provides the highest level of power conditioning and power protection for critical business IT systems, such as network equipment and business servers.

Standardize your deployments around the world and bring them online faster with the Vertiv™ VR rack. The Vertiv VR is delivered ready for high density environments to serve your mission critical needs. This rack gives you the flexibility you need with easy installation.

Register today and learn how industry leaders are solving today’s biggest challenges in the digital world!

Follow us on FacebookLinkedInTwitter and Instagram!
#VertivEvents #CiscoLive2022 @CiscoLive

Schedule a Meeting with a Vertiv Sales Consultant

First Name

Last Name

Email Address

Company

Contact number

Country

Zip Code

What I would like to discuss with Vertiv


Privacy Notice Consent

Having received and read this privacy notice on personal data processing (provided in accordance with Article 13 of EU Regulation 679/2016), I consent to:

The processing of my personal data for marketing purposes, including staying informed by email about industry trends, events, offers and product launches.

     Processing request ...

Thank you for your submission!
We will contact you shortly.

 

 

Follow us on Facebook, LinkedIn, Twitter and Instagram!
#VertivEvents #CiscoLive2022 @CiscoLive

PARTNERS
Overview
Consultants Corner
Partner Login

Language & Location