The page you're viewing is for English (Canada) region.

Working with our Vertiv Sales team enables complex designs to be configured to your unique needs. If you are an organization seeking technical guidance on a large project, Vertiv can provide the support you require.

Learn More

Many customers work with a Vertiv reseller partner to buy Vertiv products for their IT applications. Partners have extensive training and experience, and are uniquely positioned to specify, sell and support entire IT and infrastructure solutions with Vertiv products.

Find a Reseller

Already know what you need? Want the convenience of online purchase and shipping? Certain categories of Vertiv products can be purchased through an online reseller.


Find an Online Reseller

Need help choosing a product? Speak with a highly qualified Vertiv Specialist who will help guide you to the solution that is right for you.



Contact a Vertiv Specialist

The page you're viewing is for English (Canada) region.

Vertiv Introduces Power Extend Converter to Boost Voltage to Remote Radios at Cell Sites in North America

September 25, 2019

Vertiv™ eSure™ Power Extend Converter replaces circuit breaker and delivers voltage boost and overcurrent protection while conserving space

 

Columbus, Ohio [Sept. 25, 2019] – Today at ISE Expo, Vertiv introduced the Vertiv™ eSure™ C48/58-1000 Power Extend Converter, a compact device that economically boosts voltage up to -58 VDC to support increasing power needs of remote radio heads on cell towers. The eSure C48/58-1000 plugs into an existing DC distribution panel in the same position as a single-pole bullet circuit breaker, conserving usable space. The converter is available now across North America.

Today’s cell site infrastructure is evolving to support emerging 5G architectures, including 5G-friendly radios requiring more power at the top of cell towers. The eSure C48/58-1000 protects against voltage drops between the power system at the tower’s base and the radio at the top. If a voltage drop is significant enough, it can trigger a shutdown of the remote radio head before the equipment provider’s backup battery fully discharges. In the past, minor voltage drops have been manageable from base to tower, but the emergence of 5G and increased power demands are creating the need to boost voltage to ensure reliable, efficient cell site operation.

The eSure Power Extend Converter consumes 0U of additional rack space, in contrast to  traditional converter solutions which consume up to 4U of rack space. The eSure C48/58-1000 replaces a single-pole circuit breaker and provides the traditional overcurrent protection function of the circuit breaker.

“The transition from 3G to 4G and now to 5G is a complex, often expensive process for cellular providers,” said Scott Armul, VP of DC power and outside plant lines of business at Vertiv. “The eSure C48/58-1000 converter offers a fast and affordable technology upgrade that helps enable 5G delivery while seamlessly integrating with existing DC power and enclosure infrastructure.”

Along with space, the eSure C48/58-1000 conserves considerable energy while performing above 98 percent efficiency. Multiple units can operate in parallel to support radios requiring over 1kW of input power.

About Vertiv

Vertiv brings together hardware, software, analytics and ongoing services to ensure its customers’ vital applications run continuously, perform optimally and grow with their business needs. Vertiv solves the most important challenges facing today’s data centers, communication networks and commercial and industrial facilities with a portfolio of power, cooling and IT infrastructure solutions and services that extends from the cloud to the edge of the network. Headquartered in Columbus, Ohio, USA, Vertiv employs around 20,000 people and does business in more than 130 countries. For more information, and for the latest news and content from Vertiv, visit Vertiv.com.

CONTACT

Vince McMorrow
T +614 383 1622
E Vince.McMorrow@Fahlgren.com

Related Articles

PORTALS
Partner Login

Language & Location