The page you're viewing is for English (Canada) region.

Working with our Vertiv Sales team enables complex designs to be configured to your unique needs. If you are an organization seeking technical guidance on a large project, Vertiv can provide the support you require.

Learn More

Many customers work with a Vertiv reseller partner to buy Vertiv products for their IT applications. Partners have extensive training and experience, and are uniquely positioned to specify, sell and support entire IT and infrastructure solutions with Vertiv products.

Find a Reseller

Already know what you need? Want the convenience of online purchase and shipping? Certain categories of Vertiv products can be purchased through an online reseller.


Find an Online Reseller

Need help choosing a product? Speak with a highly qualified Vertiv Specialist who will help guide you to the solution that is right for you.



Contact a Vertiv Specialist

The page you're viewing is for English (Canada) region.

A power distribution unit (PDU) is a device with multiple outlets used for distributing power to servers and other IT equipment within the data center.

The PDU does not generate power but rather distributes power from the power source available during normal operation. In the event of an outage, an uninterruptible power supply (UPS) picks up the power load while the generator ramps up to begin providing power to the facility. The floor PDU then distributes the power to the rack PDU (rPDU). The rPDU, which is the last link in the power chain, distributes power to the IT equipment in each individual cabinet and rack.

There are two types of PDUs, the basic type and the smart type, which is also known as the intelligent type. While both can provide reliable power distribution to critical IT equipment within a rack or cabinet, smart PDUs offer several intelligent features like monitoring, managing, and controlling power consumption to multiple devices. The smart PDU provides data center professionals with remote network access to real-time critical infrastructure data to help drive informed decision making to ensure maximum availability and to meet important efficiency requirements.

The smart PDUs are classified into monitored and switched. Monitored PDUs provide a comprehensive view of power usage, both at the rack and via remote access and offer quick access to critical information to evaluate energy usage trends. Monitored PDUs also provide alarming capabilities to alert users of breaches in user-defined power thresholds. Switched PDUs are monitored PDUs with the added ability to remotely turn on, turn off, or reboot power at each outlet.

When selecting a PDU, organizations should consider their power requirements, their data center space, and the level of power monitoring or management their facilities require. They should take note of the services being offered by the Original Equipment Manufacturer (OEM) of the PDU that can simplify deployment and management of critical power system assets. Some vendors provide as much as a 5-year protection plan to support the life cycle of PDUs.

 

PORTALS
Partner Login

Language & Location