The page you're viewing is for English (Canada) region.

Working with our Vertiv Sales team enables complex designs to be configured to your unique needs. If you are an organization seeking technical guidance on a large project, Vertiv can provide the support you require.

Learn More

Many customers work with a Vertiv reseller partner to buy Vertiv products for their IT applications. Partners have extensive training and experience, and are uniquely positioned to specify, sell and support entire IT and infrastructure solutions with Vertiv products.

Find a Reseller

Already know what you need? Want the convenience of online purchase and shipping? Certain categories of Vertiv products can be purchased through an online reseller.


Find an Online Reseller

Need help choosing a product? Speak with a highly qualified Vertiv Specialist who will help guide you to the solution that is right for you.



Contact a Vertiv Specialist

The page you're viewing is for English (Canada) region.

High Density Reliable Power Protection for Research and Development in Data Center Lab Operations

October 31, 2023

Background

End user needed highly efficient, robust power back up and protection for their research and development centers and datacenters which required reliable power solutions that could be easily scaled and maintained along with high power usage effectiveness (PUE). However, the solutions provided by our competitors were not cost effective and utilized more footprint than required. Keeping in mind the stringent project timeline Vertiv could provide the solutions.

Results

  • Overall footprint was saved by 30%
  • Saved cost of the electrical network infrastructure (Extensive savings in Cable usage)
  • Significant savings of capital expenditure (CAPEX) and day to day expenses (OPEX)
  • Built in I/P and O/P (optional) switchgear which eliminated external panels.
  • Saved time for installation and commissioning (needed 1 week for 3000 kVA installation)
  • Reliability and efficiency improvement

 

Case Summary
Location:​

Hyderabad, India

Critical Need:

Ensure the availability of critical research and development labs and datacenters while improving energy efficiency within the existing data center footprint in order to meet growing demand without a physical expansion

Vertiv Solution:
  • Vertiv™ Liebert® Trinergy Cube
  • Vertiv™ Liebert® APM Plus
Download the Case Study
PORTALS
Partner Login

Language & Location