The page you're viewing is for English (Canada) region.

Working with our Vertiv Sales team enables complex designs to be configured to your unique needs. If you are an organization seeking technical guidance on a large project, Vertiv can provide the support you require.

Learn More

Many customers work with a Vertiv reseller partner to buy Vertiv products for their IT applications. Partners have extensive training and experience, and are uniquely positioned to specify, sell and support entire IT and infrastructure solutions with Vertiv products.

Find a Reseller

Already know what you need? Want the convenience of online purchase and shipping? Certain categories of Vertiv products can be purchased through an online reseller.


Find an Online Reseller

Need help choosing a product? Speak with a highly qualified Vertiv Specialist who will help guide you to the solution that is right for you.



Contact a Vertiv Specialist

The page you're viewing is for English (Canada) region.

Vertiv™ Liebert® DSE Freecooling System: Efficient Pumped Refrigerant Economization Without Using Water

17-12-15

The Vertiv™ Liebert® DSE is the industry's first pumped refrigerant economization system designed specifically for data centers.

Ideal for companies seeking sustainable solutions, it provides up to 50% higher efficiency than traditional systems - and it uses no water. Its advanced controls automate economization to get the most free cooling in any environment.

This white paper describes:

  • How the Liebert DSE pumped refrigerant system works
  • Advantages of pumped refrigerant economization over other technologies
  • Calculated and actual energy savings provided by the system
Download the White Paper
PORTALS
Partner Login

Language & Location