The page you're viewing is for English (Canada) region.

Working with our Vertiv Sales team enables complex designs to be configured to your unique needs. If you are an organization seeking technical guidance on a large project, Vertiv can provide the support you require.

Learn More

Many customers work with a Vertiv reseller partner to buy Vertiv products for their IT applications. Partners have extensive training and experience, and are uniquely positioned to specify, sell and support entire IT and infrastructure solutions with Vertiv products.

Find a Reseller

Already know what you need? Want the convenience of online purchase and shipping? Certain categories of Vertiv products can be purchased through an online reseller.


Find an Online Reseller

Need help choosing a product? Speak with a highly qualified Vertiv Specialist who will help guide you to the solution that is right for you.



Contact a Vertiv Specialist

The page you're viewing is for English (Canada) region.

Take a look at these four new cooling upgrade scenarios that show you how you could improve your data center's efficiency and protection. Each scenario shows you the build-out costs for the upgrade, energy savings and payback periods. Boosting the efficiency and performance to your data center might be easier and less costly than you think.

Annual Energy Savings: $333,000 
Payback Period: Under 4 Years

Scenario:

  • 1MW Data Center in Columbus, Ohio
  • Raised Floor
  • 14 rows of 14 racks
  • 17 older Liebert® Deluxe System™/3 cooling units

Challenges:

The cooling units are 15-years old or more — multiple generations out. You've been making them last and you hope to keep making them last. But money is tight and you don't see a path forward using retrofits or replacements.

Solution:

  • Replace old units with new Liebert® DSE™ free-cooling units which have advanced Liebert iCOM™ unit controls
  • Add Liebert iCOM™-S system controls to manage multiple units for higher efficiency
  • Add aisle containment for higher density and efficiency
Read the Application Note

Annual Energy Savings: $135,000 
Payback Period: 19 Months

Scenario:

  • 1MW Data Center in Columbus, Ohio
  • Raised Floor
  • 14 rows of 14 racks
  • 16 older Liebert® DS™ Cooling Systems

Challenges

The units are less than ten years old and you’ve kept them serviced on a regular basis, so they should be running well. But you want to consider improving their efficiency.

Solution

  • Add variable speed EC fans or variable speed drives
  • Replace old unit controls with advanced Liebert iCOM™ unit controls
  • Add Liebert iCOM™-S system controls to manage multiple units
  • Add aisle containment
Read the Application Note

Annual Energy Savings: $125,000 
Payback Period: 2.1 Years

Scenario:

  • 1MW Data Center in Columbus, Ohio
  • Raised Floor
  • 14 rows of 14 racks
  • 16 older Liebert® Deluxe System/3 Units

Challenges

The cooling units are 15 years old and you plan to replace them in five years. Until then, you’d consider an upgrade strategy, if you could recoup your investment between now and then.

Solution:

  • Option 1: You can retrofit components to add another five years to the life of the
    equipment beyond the planned replacement date
  • Option 2: You can replace the old equipment with new and more efficient units, and still achieve a payback within your 5-year timeframe
Read the Application Note

Annual Energy Savings: $55,000 
Payback Period: 18 Months

Scenario:

  • 1MW Data Center in Columbus, Ohio
  • Raised Floor
  • 14 rows of 14 racks
  • 10 new Liebert DSE free-cooling unit

Challenges

You have new cooling economization equipment with no pressing need for upgrading. In this case, you’re using the ultra-efficient Liebert DSE free-cooling economization system with advanced unit controls. Still, you want to consider ways to improve efficiency.

Solution

  • Add Liebert iCOM-S system controls to harmonize the operation of multiple units for higher efficiency
  • Add aisle containment for higher density and efficiency
Read the Application Note

PORTALS
Partner Login

Language & Location