The page you're viewing is for English (Canada) region.

Working with our Vertiv Sales team enables complex designs to be configured to your unique needs. If you are an organization seeking technical guidance on a large project, Vertiv can provide the support you require.

Learn More

Many customers work with a Vertiv reseller partner to buy Vertiv products for their IT applications. Partners have extensive training and experience, and are uniquely positioned to specify, sell and support entire IT and infrastructure solutions with Vertiv products.

Find a Reseller

Already know what you need? Want the convenience of online purchase and shipping? Certain categories of Vertiv products can be purchased through an online reseller.


Find an Online Reseller

Need help choosing a product? Speak with a highly qualified Vertiv Specialist who will help guide you to the solution that is right for you.



Contact a Vertiv Specialist

The page you're viewing is for English (Canada) region.

Custom Mobile Backup Protects Communication Provider's Networks

18-11-28

Never knowing when and where a disaster might occur, this company required that the mobile backup unit be easy to transport and maintain, and designed to operate in extreme environments.

About the Company

This communications provider is a leader in broadband satellite technology and services, serving more than one million customers in North and South America.

Background

A leading provider of satellite-based communications systems needed a mobile disaster recovery unit to support its terrestrial network in the event of a fixed facility failure. Never knowing when and where a disaster might occur, this company required that the mobile backup unit be easy to transport and maintain, and designed to operate in extreme environments.

Specializing in critical technologies that always work, Vertiv designed a custom trailer-mounted SmartMod™ solution with an internal sliding rail system for easy access to keep their backup system always ready. The trailer solution offers a quick-connect system for power and signal, as well as DX-based condensers mounted on the trailer. It delivered a backup infrastructure with a constant “ready for service” state that exceeded the communication company’s needs.

Our SmartMod is a modular, customized data center enclosure. It is a fully integrated, self-contained, rapidly deployable system that’s adaptable, flexible, and efficient. The compact nature of the SmartMod allows for easy transportation without compromising functionality or long-term value.

Case Summary

Location: Varies

Critical Need: A communications provider needed a mobile disaster recovery unit to support their terrestrial network in the event of a fixed facility failure.

Product/Service: SmartMod infrastructure provides intelligent, rapidly deployable, prefabricated enclosures for modular data centers, cable landing stations, or network aggregation.

Results:

  • Designed a trailer-mounted SmartMod with a proprietary internal sliding rail system for easy access to equipment
  • Equipped with quick-connect systems for power and signal as well as DX-based condensers mounted on the trailer
  • Provided an easy to maintain, durable solution to keep back-up in constant “ready for service” state
  • Created a mobile environment, easily used wherever a need arises
Download the Case Study
PORTALS
Partner Login

Language & Location