The page you're viewing is for English (Canada) region.

Working with our Vertiv Sales team enables complex designs to be configured to your unique needs. If you are an organization seeking technical guidance on a large project, Vertiv can provide the support you require.

Learn More

Many customers work with a Vertiv reseller partner to buy Vertiv products for their IT applications. Partners have extensive training and experience, and are uniquely positioned to specify, sell and support entire IT and infrastructure solutions with Vertiv products.

Find a Reseller

Already know what you need? Want the convenience of online purchase and shipping? Certain categories of Vertiv products can be purchased through an online reseller.


Find an Online Reseller

Need help choosing a product? Speak with a highly qualified Vertiv Specialist who will help guide you to the solution that is right for you.



Contact a Vertiv Specialist

The page you're viewing is for English (Canada) region.

Felix Telecom Strengthens Security by Upgrading Network Infrastructure in Romania

24-7-11

Background:  

When a pivotal organization in the Romanian public sector contacted Felix Telecom to upgrade its communications and surveillance equipment, they chose Vertiv to help accomplish this goal.   

The two partners upgraded the organization’s telecommunication network with new power technology and supporting infrastructure, including AC-powered data and security equipment and DC-powered radio equipment.   

Results:

  • Installed the Vertiv™ NetSure™ Inverter System at 300 sites over six months
  • Gained a minimum of four hours of battery backup, with 500W of AC load and 3 kW of DC load
  • Implemented a space-saving solution that can easily be extended in the future
  • Created a repeatable concept that will now be used in other countries
Case Summary
​Location:​

Bucharest, Romania

Critical Need:

As security operations require continual equipment availability, the organization sought to deploy a power distribution solution that would provide battery backup capabilities when local utilities experienced unplanned downtime. Additionally, the organization sought to rapidly deploy a converged network while also minimizing costs. 

Vertiv Solution:

Vertiv™ NetSure™ Inverter System

DOWNLOAD THE CASE STUDY

385x872-Felix CS image.jpg

PORTALS
Partner Login

Language & Location