The page you're viewing is for English (Canada) region.

Working with our Vertiv Sales team enables complex designs to be configured to your unique needs. If you are an organization seeking technical guidance on a large project, Vertiv can provide the support you require.

Learn More

Many customers work with a Vertiv reseller partner to buy Vertiv products for their IT applications. Partners have extensive training and experience, and are uniquely positioned to specify, sell and support entire IT and infrastructure solutions with Vertiv products.

Find a Reseller

Already know what you need? Want the convenience of online purchase and shipping? Certain categories of Vertiv products can be purchased through an online reseller.


Find an Online Reseller

Need help choosing a product? Speak with a highly qualified Vertiv Specialist who will help guide you to the solution that is right for you.



Contact a Vertiv Specialist

The page you're viewing is for English (Canada) region.

Dedicated IT cooling: Keeping servers reliable across industries

•

Across hospitals, banks, and government offices, small server rooms now sustain critical operations, handling patient records, financial data, and citizen services. Many enterprises, however, still rely on comfort cooling meant for people, not for IT equipment that runs nonstop. That gap in the thermal chain is where outages begin.

One in eight outages are caused by cooling failures.1

1Donnellan, D., Lawrence, A., & Weinschenk, R. (2025). Annual outage analysis 2025. Uptime Institute. https://uptimeinstitute.com/resources/research-and-reports/annual-outage-analysis-2025.

Cooling built for constant IT demand keeps systems steady where comfort cooling units fall short. Dedicated IT cooling anchors a unified thermal chain—linked with power and monitoring for true reliability. Together, these end-to-end systems and services protect uptime today and scale with tomorrow’s workloads.

 

Finance: Cooling that safeguards capital reserves

Finance IT systems rely on information to execute strategic decisions. Whether in trading or in banking transactions, uptime is critical to avoid missed opportunities and unnecessary delays.

Financial firms operate on digital platforms, utilizing tools such as real-time trading, payment processing, account management, loan origination, and risk analytics. Finance servers process transactions, enable connectivity to payment networks, stock exchange, and other financial institutions with minimal latency.

Tracking the cost of finance interruptions

According to a report by New Relic, outages occurred more in the finance industry than in many other sectors. In the same report, the respondents noted:

48%

experienced outages at least once a week

58%

respondents said that it takes at least 30 minutes to detect high impact outages

71%

said it takes at least 30 minutes to resolve it

71%

said critical outages cost at least $1 million per hour of downtime.

What’s at stake when thermal falls behind

When cooling lags, customer apps and banking systems can stall and require reconciliation. Real deployments show why right-sized, responsive cooling matters—variable-speed systems that track changing loads help protect uptime and reduce energy use.
The impact isn’t limited to hardware. When thermal performance slips, organizations face:

  • Negative customer experiences that erode trust during service interruptions.
  • Brand and regulatory exposure from prolonged disruption.

See Vertiv solutions for finance.

Strategic imperatives

Advancing thermal systems for uptime

Thermal management must evolve from a single-focus task into a comprehensive strategy. Network closets and server rooms with comfort cooling systems can’t be utilized in the thermal chain since office-grade air conditioning (AC) isn’t designed to run 24/7.

Design for density

Utilize dedicated IT cooling that targets the heat source to prevent overheating of finance servers.

Maximize efficiency

Workloads spike unpredictably. Real-time thermal controls and unified monitoring help avoid stranded capacity and improve uptime.

Monitor for resilience

Downtime is costly. Use predictive diagnostics and automated alerts to catch thermal issues early.

Thermal risk summary

Best practices for IT resilience

Financial services run continuously. Branches, ATMs, payments, and trading links create steady heat in server rooms and network closets. Many sites still depend on comfort AC that cycles with occupancy or thermostat settings, has low sensible cooling and limited airflow control, and lacks proactive monitoring. The result: hot spots, after-hours temperature drift, and preventable incidents that slow down services, eroding trust.

To close the gap:

  • Maintain 24×7x365 IT-appropriate temperature and humidity.
  • Improve airflow management:
    • Use hot/cold aisle layouts,
    • Place units near heat sources, or
    • Apply ducting to separate supply and return air.
  • Add environmental sensing with remote alerts.
  • Use a standardized branch thermal checklist/playbook.
  • Run scheduled thermal walk-throughs and load tests, with simple reporting to track drift and incidents.

Government: Cooling that enables uninterrupted governance

Government IT systems support essential public services and national operations. From managing citizen data to coordinating emergency response, uptime is critical to support continuity and public trust.

Government agencies rely on digital platforms to deliver services such as identity management, benefits distribution, tax processing, law enforcement coordination, and geographic information systems (GIS). These systems enable secure data exchange across departments, support real-time decision-making, and maintain connectivity with national databases and external partners—all with strict latency and security requirements.

PORTALS
Partner Login

Language & Location