Sorry, this page isn't available for your location.

The page you're viewing is for Portuguese (EMEA) region.

Trabalhar com um representante do fabricante Vertiv permite que os designs complexos sejam configurados de acordo com as suas necessidades únicas. Se for uma organização que procura orientação técnica num projeto de grandes dimensões, a Vertiv pode fornecer o apoio de que necessita.

Saiba mais

Muitos clientes trabalham com um parceiro revendedor Vertiv, para comprar produtos Vertiv para as suas aplicações de IT. Os parceiros têm uma vasta formação e experiência, e estão posicionados de forma única para especificar, vender e apoiar soluções completas de TI e infraestruturas com produtos Vertiv.

Encontrar um revendedor

Já sabe do que precisa? Quer a conveniência da compra e do envio online? Determinadas categorias de produtos Vertiv podem ser adquiridas através de um revendedor online.


Encontre um revendedor on-line

Precisa de ajuda para escolher um produto? Fale com um Especialista Vertiv altamente qualificado que o ajudará a orientar-se para a solução certa para si.



Contacte um Especialista Vertiv

Sorry, this page isn't available for your location.

The page you're viewing is for Portuguese (EMEA) region.

Inwi scales cooling performance at Technopolis Data Centre Site with Vertiv chilled water solutions

abril 28, 2026

Rabat, Morocco [28 April, 2026] – Following the successful deployment of thermal management solutions at its Marrakech and Settat data centres, leading Moroccan telecommunications provider Inwi has once again relied on Vertiv, a global leader in critical digital infrastructure, this time to support expansion at its Technopolis Rabat facility, with an emphasis on cooling efficiency, redundancy and resilience. Africa’s fast-growing digital economy depends on reliable data centre infrastructure to support cloud services, mobile networks and digital innovation, and Inwi and its data centres play a pivotal role in enabling this foundation.

The project at Inwi’s Technopolis Rabat site focused on upgrading cooling capabilities using advanced chilled water systems and precision cooling units, building on the proven performance delivered by Vertiv at the Marrakech and Settat facilities. This particular implementation brought with it a unique set of technical challenges, particularly the need to maintain optimal cooling efficiency in high ambient temperatures, which can exceed 45°C during summer months. In addition, the company needed to integrate new cooling systems within its existing infrastructure without disrupting ongoing operations, while at the same time reducing its carbon footprint in alignment with Inwi’s energy efficiency goals.

To address these requirements, Vertiv installed chilled water systems, featuring the Vertiv™ Liebert® AFC air-cooled chiller with a 715 kW cooling capacity, designed with integrated free cooling capabilities and configured with both a main and redundant unit to enable continuous data centre operations during system maintenance or other downtime. The solution also includes Vertiv™ Liebert® PCW CRAH units with chilled water cooling, designed for IT rooms to maintain consistent temperature and humidity, integrated with Vertiv™ Liebert® iCOM™ control systems for real-time performance optimisation and efficient temperature management. In addition, Vertiv provided lifecycle services including installation and commissioning, technical consultancy to design a cooling system aligned with Inwi’s operational requirements, and ongoing maintenance and support for optimal system performance over the long term.

The result is a cooling infrastructure designed to allow for performance, efficiency and growth. Reliability at the Technopolis Rabat site has been enhanced through cooling systems that safeguard uptime and operational stability. At the same time, efficiency has been improved through free-cooling capabilities that reduce energy use and operating costs. Resilience was strengthened through N+1 redundancy, maintaining availability during component failures, and scalability has been achieved through a modular design that supports future growth without disruption.

“By implementing advanced chilled water and precision cooling solutions at our Technopolis Rabat site, Vertiv has played a key role in our strategic initiative to upgrade and modernise Inwi’s data centre facilities, enabling us to meet the growing demands for data processing and storage,” says Abdelilah Idrissi, head of data centers design & operations at Inwi.

“Africa is undergoing a significant transformation in both its energy and digital infrastructure sectors, and the continent's increasing demand for advanced digital infrastructure aligns with Vertiv's expertise in enabling resilient, critical infrastructure technologies,” states Zineb Kamri, Vertiv’s regional director for Northwest Africa. “Vertiv’s consistent delivery of high-quality infrastructure solutions and technical support has positioned us as a preferred supplier for Inwi’s data centre projects. The success of the Marrakech and Settat installations paved the way for this new opportunity at Technopolis, reinforcing our position as a trusted provider for cutting-edge infrastructure solutions tailored to Inwi’s evolving needs.”

For more information on Vertiv and its portfolio of infrastructure solutions and services, please click here.

About Vertiv

Vertiv (NYSE: VRT) brings together hardware, software, analytics and ongoing services to enable its customers’ vital applications to run continuously, perform optimally and grow with their business needs. Vertiv solves the most important challenges facing today’s data centers, communication networks and commercial and industrial facilities with a portfolio of power, cooling and IT infrastructure solutions and services that extends from the cloud to the edge of the network. Headquartered in Westerville, Ohio, USA, Vertiv does business in more than 130 countries. For more information, and for the latest news and content from Vertiv, visit Vertiv.com.

Forward-looking statements

This release contains forward-looking statements within the meaning of the Private Securities Litigation Reform Act of 1995, Section 27 of the Securities Act, and Section 21E of the Securities Exchange Act. These statements are only a prediction. Actual events or results may differ materially from those in the forward-looking statements set forth herein. Readers are referred to Vertiv’s filings with the Securities and Exchange Commission, including its most recent Annual Report on Form 10-K and any subsequent Quarterly Reports on Form 10-Q for a discussion of these and other important risk factors concerning Vertiv and its operations. Vertiv is under no obligation to, and expressly disclaims any obligation to, update or alter its forward-looking statements, whether as a result of new information, future events or otherwise.

VERTIV MEDIA CONTACT

E icomm@pr.co.za

Acesso de Partner

Idioma e Localização