Sorry, this page isn't available for your location.

The page you're viewing is for Portuguese (EMEA) region.

Trabalhar com um representante do fabricante Vertiv permite que os designs complexos sejam configurados de acordo com as suas necessidades únicas. Se for uma organização que procura orientação técnica num projeto de grandes dimensões, a Vertiv pode fornecer o apoio de que necessita.

Saiba mais

Muitos clientes trabalham com um parceiro revendedor Vertiv, para comprar produtos Vertiv para as suas aplicações de IT. Os parceiros têm uma vasta formação e experiência, e estão posicionados de forma única para especificar, vender e apoiar soluções completas de TI e infraestruturas com produtos Vertiv.

Encontrar um revendedor

Já sabe do que precisa? Quer a conveniência da compra e do envio online? Determinadas categorias de produtos Vertiv podem ser adquiridas através de um revendedor online.


Encontre um revendedor on-line

Precisa de ajuda para escolher um produto? Fale com um Especialista Vertiv altamente qualificado que o ajudará a orientar-se para a solução certa para si.



Contacte um Especialista Vertiv

Sorry, this page isn't available for your location.

The page you're viewing is for Portuguese (EMEA) region.

Now available across EMEA, the Vertiv™ Edge Lithium-Ion UPS models provide longer battery life and runtime and deliver lowest total cost of ownership

London, UK [October 7, 2021] – Vertiv (NYSE: VRT), a global provider of critical digital infrastructure and continuity solutions, today announced the availability of single phase uninterruptible power supply (UPS) systems with lithium-ion battery models, expanding its portfolio of line-interactive UPS. With capacities ranging from 1500 – 3000VA in tower and rack-mount convertible designs, the highly-efficient single-phase Vertiv™ Edge Lithium-Ion UPS family is now available across Europe, the Middle East and Africa (EMEA).

Thanks to their lower maintenance requirements, lithium-ion batteries (also known as Li-ion or LIB) are a natural fit for deployments at the edge of the network, where IT support is limited. Compared with valve-regulated lead acid (VRLA) batteries, lithium-ion batteries have up to 3x longer life, which improves total cost of ownership (TCO). Moreover, they perform with greater efficiencies at higher temperatures, are smaller, lighter and deliver longer runtimes than VRLA batteries used for UPS systems in these capacities. The Vertiv Edge Lithium-Ion UPS family provides up to 10 minutes of battery backup at full load, as opposed to approximately 4-5 minutes for a standard UPS with VRLA batteries.

“As digitalisation increases, many applications are moving to the edge of the network and require reliable power protection,” said Karsten Winther, vice president sales for Vertiv in EMEA. “UPS systems with lithium-ion batteries offer cost and operation benefits, and also reduce the need for on-site maintenance. Ultimately this means more stability and savings for critical edge deployments, and a wider range of options for our customers.”

The Vertiv Edge Lithium-Ion UPS is ideal for edge computing sites and for healthcare, banking, education, retail and government applications. It comes with a standard five-year warranty on the electronics and battery. The system can be integrated with the Vertiv™ VR Rack for a standardized IT infrastructure solution that can be easily deployed across various edge locations.

The Vertiv™ Edge Lithium-Ion UPS family is supported by Vertiv™ Power Insight software, available as a free download on Vertiv’s website. Vertiv Power Insight allows users to easily monitor and manage up to 100 rack power distribution units (rPDUs) and UPS systems, with shutdown protection for individual and virtual servers, providing increased visibility and better management of multiple edge locations. 

To learn more about using lithium-ion batteries with single-phase UPS systems, download the Vertiv white paper, The Advantages of Using Lithium-Ion Batteries as A Backup Power Source in Single-Phase UPS Applications for Remote and Edge Data Centres. For more information on the Vertiv Edge Lithium-ion and other UPS systems from Vertiv, visit Vertiv.com.

About Vertiv

Vertiv (NYSE: VRT) brings together hardware, software, analytics and ongoing services to ensure its customers’ vital applications run continuously, perform optimally and grow with their business needs. Vertiv solves the most important challenges facing today’s data centers, communication networks and commercial and industrial facilities with a portfolio of power, cooling and IT infrastructure solutions and services that extends from the cloud to the edge of the network. Headquartered in Columbus, Ohio, USA, Vertiv employs approximately 21,000 people and does business in more than 130 countries. For more information, and for the latest news and content from Vertiv, visit Vertiv.com.

Forward-Looking Statements

This release contains forward-looking statements within the meaning of the Private Securities Litigation Reform Act of 1995, Section 27 of the Securities Act, and Section 21E of the Securities Exchange Act. These statements are only a prediction. Actual events or results may differ materially from those in the forward-looking statement set forth herein. Readers are referred to Vertiv’s filings with the Securities and Exchange Commission, including its most recent Annual Report on Form 10-K/A and any subsequent Quarterly Reports on Form 10-Q for a discussion of these and other important risk factors concerning Vertiv and its operations. Vertiv is under no obligation to, and expressly disclaims any obligation to, update or alter its forward-looking statements, whether as a result of new information, future events or otherwise.

MEDIA CONTACT

Chris Kader
T +44 7941 499877
E ckader@mww.com

Artigos relacionados

Acesso de Partner

Idioma e Localização