The page you're viewing is for Portuguese (EMEA) region.

Trabalhar com um representante do fabricante Vertiv permite que os designs complexos sejam configurados de acordo com as suas necessidades únicas. Se for uma organização que procura orientação técnica num projeto de grandes dimensões, a Vertiv pode fornecer o apoio de que necessita.

Saiba mais

Muitos clientes trabalham com um parceiro revendedor Vertiv, para comprar produtos Vertiv para as suas aplicações de IT. Os parceiros têm uma vasta formação e experiência, e estão posicionados de forma única para especificar, vender e apoiar soluções completas de TI e infraestruturas com produtos Vertiv.

Encontrar um revendedor

Já sabe do que precisa? Quer a conveniência da compra e do envio online? Determinadas categorias de produtos Vertiv podem ser adquiridas através de um revendedor online.


Encontre um revendedor on-line

Precisa de ajuda para escolher um produto? Fale com um Especialista Vertiv altamente qualificado que o ajudará a orientar-se para a solução certa para si.



Contacte um Especialista Vertiv

The page you're viewing is for Portuguese (EMEA) region.

The Vertiv™ CoolPhase Perimeter, Vertiv™ CoolPhase Row, and Vertiv™ CoolPhase Wall systems are now available with low-GWP refrigerant options, maintaining performance and reliability while supporting regulatory compliance ahead of 2027 North America deadlines

COLUMBUS, Ohio [October 2, 2025] – Vertiv (NYSE: VRT), a global leader in critical digital infrastructure, today announced the North America availability of low-GWP refrigerant versions of its perimeter, row, and wall-mount cooling systems for data centers. These systems are part of Vertiv’s direct expansion (DX) thermal management portfolio and are available more than a year in advance of U.S. EPA requirements taking effect on January 1, 2027.  Further, they are fully compliant with current California regulations as well as with impending New York state regulations that take effect in January 2026.

The newly released Vertiv™ CoolPhase Perimeter uses R-454B refrigerant, a low-GWP alternative to legacy refrigerants that reduces environmental impact while complying with regulatory requirements. The Vertiv™ CoolPhase Row and Vertiv™ CoolPhase Wall use R-32 refrigerant, also classified as low-GWP, supporting compliance while maintaining performance. The systems are designed to maintain or even improve footprint, performance, reliability, and efficiency compared to the legacy Vertiv™ Liebert® DS, Vertiv™ Liebert® DSE, Vertiv™ Liebert® PDX, and Vertiv™ Liebert® CRV units. With Vertiv™ Liebert® iCOM™ controls integration and smart design, the new Vertiv™ CoolPhase systems deliver energy efficiency while maintaining the performance customers expect.

“Customers looking to stay ahead of regulatory deadlines can start that journey today,” said Ben Smith, vice president of thermal management at Vertiv. “The Vertiv CoolPhase Perimeter, Vertiv CoolPhase Row, and Vertiv CoolPhase Wall systems give operators a straightforward path to replace older models with low GWP compliant, energy efficient solutions that align with environmental goals while providing the needed performance and reliability.”

These systems further strengthen Vertiv’s thermal portfolio, which spans air handlers, direct expansion, chillers, in-room cooling, rear-door heat exchangers, and liquid cooling. The low GWP offerings reinforce Vertiv’s position as a partner delivering energy efficient solutions across data center environments.

For more information on Vertiv™ CoolPhase low-GWP systems and Vertiv’s full portfolio of end-to-end thermal and power management solutions, visit Vertiv.com.

About Vertiv

Vertiv (NYSE: VRT) brings together hardware, software, analytics and ongoing services to enable its customers’ vital applications to run continuously, perform optimally and grow with their business needs. Vertiv solves the most important challenges facing today’s data centers, communication networks and commercial and industrial facilities with a portfolio of power, cooling and IT infrastructure solutions and services that extends from the cloud to the edge of the network. Headquartered in Westerville, Ohio, USA, Vertiv does business in more than 130 countries. For more information, and for the latest news and content from Vertiv, visit Vertiv.com.

Forward-looking statements

This release contains forward-looking statements within the meaning of the Private Securities Litigation Reform Act of 1995, Section 27 of the Securities Act, and Section 21E of the Securities Exchange Act. These statements are only a prediction. Actual events or results may differ materially from those in the forward-looking statements set forth herein. Readers are referred to Vertiv’s filings with the Securities and Exchange Commission, including its most recent Annual Report on Form 10-K and any subsequent Quarterly Reports on Form 10-Q for a discussion of these and other important risk factors concerning Vertiv and its operations. Vertiv is under no obligation to, and expressly disclaims any obligation to, update or alter its forward-looking statements, whether as a result of new information, future events or otherwise.

 

CONTACT
Ruder Finn
E 
Vertiv@RuderFinn.com

Artigos relacionados

Idioma e Localização