Sorry, this page isn't available for your location.

The page you're viewing is for Portuguese (EMEA) region.

Trabalhar com um representante do fabricante Vertiv permite que os designs complexos sejam configurados de acordo com as suas necessidades únicas. Se for uma organização que procura orientação técnica num projeto de grandes dimensões, a Vertiv pode fornecer o apoio de que necessita.

Saiba mais

Muitos clientes trabalham com um parceiro revendedor Vertiv, para comprar produtos Vertiv para as suas aplicações de IT. Os parceiros têm uma vasta formação e experiência, e estão posicionados de forma única para especificar, vender e apoiar soluções completas de TI e infraestruturas com produtos Vertiv.

Encontrar um revendedor

Já sabe do que precisa? Quer a conveniência da compra e do envio online? Determinadas categorias de produtos Vertiv podem ser adquiridas através de um revendedor online.


Encontre um revendedor on-line

Precisa de ajuda para escolher um produto? Fale com um Especialista Vertiv altamente qualificado que o ajudará a orientar-se para a solução certa para si.



Contacte um Especialista Vertiv

Sorry, this page isn't available for your location.

The page you're viewing is for Portuguese (EMEA) region.

Vertiv Introduces New Line of Rack Transfer Switches and Lithium-Ion Uninterruptible Power Supply for Distributed IT and Network Edge Computing Applications in EMEA

15/11/22

New series of power products further expand Vertiv’s offering dedicated to IT channel partners

London, UK [November 15, 2022] - Vertiv (NYSE: VRT), a global provider of critical digital infrastructure and continuity solutions, today introduced the Vertiv™ Geist™ Rack Transfer Switch (RTS), a new line of transfer switches that provides redundant power to single-corded devices, and the highly-efficient Vertiv™ Liebert® GXT5 Lithium-Ion uninterruptible power supply (UPS), designed for rack or stand-alone installation. These space-saving devices are ideal for use in distributed IT networks and edge computing locations, and are now available and shipping from stock in Europe, Middle East and Africa (EMEA).

The Vertiv Geist RTS instantly detects loss of power and automatically switches the load to an alternative source in less than 4 to 8 milliseconds, allowing the supported servers and other critical devices to continue to operate through a planned or unplanned outage. It is currently available in basic upgradeable and enhanced intelligence models, as well as switched and outlet-level monitored models. Basic upgradeable models include the intelligence needed today, with the option to upgrade technology as needs evolve. Enhanced intelligence models provide a comprehensive view of critical IT equipment power usage, available either at the rack or via remote access.

In addition to providing redundant power, the Vertiv Geist RTS also proactively monitors the IT environment, including temperature, humidity, and airflow. Users have the option to enhance device monitoring features, with remote monitoring of IT power usage. The Vertiv Geist RTS can support up to 24 outlets for higher-density rack configurations.

Available in 1000VA, 1500VA, 2000VA and 3000VA capacities, the Liebert GXT5 Lithium-Ion is a double-conversion, online UPS which leverages the higher power density of lithium-ion to pack more battery runtime in the same amount of space as a typical valve-regulated lead acid (VRLA) battery. The Liebert® GXT5 Lithium-Ion also supports scalable runtime with the ability to add up to eight 1U lithium-ion external battery cabinets to each UPS.

Lithium-ion batteries typically last 8-10 years – roughly the lifespan of the UPS itself – compared to about 3-5 years for VRLA batteries, potentially eliminating costly and inconvenient battery replacements and maintenance. Lithium-ion batteries are also significantly lighter than VRLA batteries and perform better at higher temperatures, reducing the expenses and energy required for rack cooling. These inherent benefits give Liebert GXT5 Lithium-Ion customers a total cost of ownership (TCO) that is up to 50% lower than a similar UPS using VRLA batteries, during the typical life of the UPS. Moreover, the Liebert GXT5 Lithium-Ion features a high power factor (0.9-1.0) and efficiency up to 95% in online mode and up to 98% in active ECO mode, enabling further savings on energy and costs.

“As edge computing, IoT and 5G continue to expand and become the new backbone of digitalisation, distributors and resellers are looking for efficient solutions to protect small and micro IT sites against power outages,” said Birgit Jackson, director, integrated racks and IT solutions for Vertiv in EMEA. “These additions to our IT channel portfolio bring a series of benefits to support growth at the edge of the network, enabling businesses to leverage latest technologies and accelerate their digital transformation journey.”

The Vertiv™ Geist™ RTS and Liebert GXT5 Lithium-Ion UPS are ideal for banking, healthcare, financial services, education, energy, government and transportation industries that operate micro data centres, distributed IT networks or edge computing data centres.  

These latest additions to Vertiv’s IT channel portfolio enable EMEA resellers in participating countries to earn more points through the Vertiv Incentive Programme (VIP), which allows partners to easily win rewards without the need for any reporting. Bonus points are uploaded into the Vertiv Partner Portal monthly, and the partner only needs to log in to redeem them.

For more information about Vertiv and its channel portfolio, visit Vertiv.com. Click on “Partners” and “Apply Now” to take full advantage of what Vertiv has to offer.

About Vertiv

Vertiv (NYSE: VRT) brings together hardware, software, analytics and ongoing services to enable its customers’ vital applications to run continuously, perform optimally and grow with their business needs. Vertiv solves the most important challenges facing today’s data centres, communication networks and commercial and industrial facilities with a portfolio of power, cooling and IT infrastructure solutions and services that extends from the cloud to the edge of the network. Headquartered in Columbus, Ohio, USA, Vertiv employs approximately 24,000 people and does business in more than 130 countries. For more information, and for the latest news and content from Vertiv, visit Vertiv.com.

Forward-Looking Statements

This release contains forward-looking statements within the meaning of the Private Securities Litigation Reform Act of 1995, Section 27 of the Securities Act, and Section 21E of the Securities Exchange Act. These statements are only a prediction. Actual events or results may differ materially from those in the forward-looking statements set forth herein. Readers are referred to Vertiv’s filings with the Securities and Exchange Commission, including its most recent Annual Report on Form 10-K and any subsequent Quarterly Reports on Form 10-Q for a discussion of these and other important risk factors concerning Vertiv and its operations. Vertiv is under no obligation to, and expressly disclaims any obligation to, update or alter its forward-looking statements, whether as a result of new information, future events or otherwise.

CONTACT

Susanna Collins
T: +44 (0)7872 558593
E: susanna.collins@apodpr.co.uk

Acesso de Partner

Idioma e Localização