The page you're viewing is for Japanese (Japan) region.

Vertivの製造担当者と連携すると、複雑な設計をお客様独自のニーズに合わせて構成することが可能になります。大規模なプロジェクトに関する技術的ガイドが必要な組織に対して、Vertivは十分なサポートを提供いたします。

詳細を見る

Vertiv再販業者パートナーと連携して、多くのお客様がITアプリケーション用のVertiv製品を購入しています。パートナーは、広範なトレーニングと経験を積み、ITおよびインフラに関するソリューション全体をVertiv製品で明確にし、販売、サポートを行うという独自の立場を構築しています。
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
Battery energy storage systems

What is a BESS (Battery Energy Storage System)

A BESS is typically comprised of battery cells arranged into modules. These modules are connected into strings to achieve the desired DC voltage. The strings are often described as racks where the modules are installed. The collected DC outputs from the racks are routed into a 4-quadrant inverter called a Power Conversions System (PCS). The PCS converts the power to AC and then routes it through transformers and switchgear where the facility or the grid can use it. A grid controller is necessary to interact with the external inputs from CT’s, PTs, and other intelligent devices.

800x450-physical-energy-storage-system.jpg

When including a BESS with a microgrid, the following grid services are possible

Voltage and Frequency Services

During the utility-connected mode of operation, a microgrid owner can utilize DERs to opt into paid service by the utility companies. This feature commands the system to assist the utility in maintaining localized grid power quality via a direct command control sequence that the controller will receive from the utility grid operator. It issues commands to one or all the DERs to respond to the requirement. Read more

Utility Demand Management

Depending on the selection of the DERs and their capability, along with the owner’s utility rate structure, a demand charge may be present that can be avoided by deft management of battery storage resources should it be part of the microgrid resources. This capability is expected to monitor and predict the client’s load and respond to daytime power consumption peaks by activating the battery’s output to avoid setting a high demand charge. This results in reduced utility costs. Read more

Time of Use Load Management

Although the microgrid controller is expected to manage the load during an islanding event, it can also do so while in grid connected mode. The controller can be configured to recommend and activate loads at various times of day when utility rates are favorable yet not overly impacting client operations. During the utility–connected mode of operation, a microgrid owner can utilize the always-on DERs in the grid to opt into paid service by the utility companies. This feature commands the system to assist the utility in maintaining localized grid power quality via a direct command control sequence that the controller will receive from the utility grid operator and issue commands to one or all of the DERs to respond to the requirement. Read more

 

BESS integration considerations

800x450-AC-Coupled-BESS.jpg

BESS utility interconnection

Integrating a BESS within the context of a microgrid with respect to the electrical utility is often like interconnecting other DER, such as generators and PV solar farms. The PCS used for the BESS will need to comply with the same standards as solar PV inverters (such as IEEE-1547-2018). The concern that the utility has, however, is possible reactive and/or short circuit power contributions the BESS could still present to the grid.

Read our white paper

Vertiv™ EnergyCore grid - Battery energy storage system, integrated modular design

The Vertiv™ EnergyCore Grid - Battery Energy Storage System uses UL9540A lithium-ion batteries to provide utility-scale energy storage for mission-critical businesses that can be used as an always-on power supply. This energy storage can be used to smooth out power usage and seamlessly transition to an always-on battery-enabled power supply whenever needed. By doing so, organizations can reduce OpEx costs, such as peak demand charges, on an ongoing basis. They can also participate in energy arbitrage and other services, enhancing profitability.

Common applications include:

  • Gaining flexible peaking capacity
  • Regulating power voltage and frequency
  • Integrating renewable energy sources
  • Enabling new grid services
  • Enhancing utility transmission and distribution reliability.

Learn more on our Vertiv™ EnergyCore Grid - Battery Energy Storage System product page

Vertiv-DynaFlex-BESSProduct-Infographic-MAIN-v2.jpg

Talk to an expert
Please complete the form below and we'll get back to you as soon as possible.


First Name

Last Name

Email Address

Phone

Company

Country

Zip code

Comment


Privacy Notice Consent

Having received and read this privacy notice on personal data processing (provided in accordance with Article 13 of EU Regulation 679/2016), I consent to:

The processing of my personal data for marketing purposes, including staying informed by email about industry trends, events, offers and product launches.

     Processing request ...

Thank you! Your submission has been sent.

Other Resources

Partner Login

言語と地域