Sorry, this page isn't available for your location.

The page you're viewing is for English (India) region.

Working with our Vertiv Sales team enables complex designs to be configured to your unique needs. If you are an organization seeking technical guidance on a large project, Vertiv can provide the support you require.

Learn More

Many customers work with a Vertiv reseller partner to buy Vertiv products for their IT applications. Partners have extensive training and experience, and are uniquely positioned to specify, sell and support entire IT and infrastructure solutions with Vertiv products.

Find a Reseller

Already know what you need? Want the convenience of online purchase and shipping? Certain categories of Vertiv products can be purchased through an online reseller.


Find an Online Reseller

Need help choosing a product? Speak with a highly qualified Vertiv Specialist who will help guide you to the solution that is right for you.



Contact a Vertiv Specialist

Sorry, this page isn't available for your location.

The page you're viewing is for English (India) region.

Vertiv Launches New Line of Local Rack Access Consoles with Integrated KVM to Simplify Data Center Management in Asia

18-11-21

VertivTM CLRA 18.5 inch local rack access console with integrated KVM require just 1U of rack space

Mumbai, India [November 18, 2021] – Vertiv (NYSE: VRT), a global provider of critical digital infrastructure and continuity solutions, today introduced a line of local rack access consoles, with models that include an integrated KVM (keyboard, video, mouse) switch. The Vertiv™ CLRA local rack access console features an 18.5 inch LCD panel and optional, integrated 8 or 16 port KVM that fits in the same 1U space, saving room while increasing management and functionality. Vertiv CLRA is now available exclusively in Asia.

The Vertiv CLRA local rack access console simplifies access and management for data center managers who are managing a single rack  or  multiple sites across different locations. The console  supports high definition video resolution and includes next-generation rails that allow seamless installation into the racks without any tools. This device allows quick and easy access to multiple servers, making software upgrades, troubleshooting and system monitoring more convenient and less time consuming.

“Data centers play a very crucial role in a world that’s becoming increasingly virtual. While organizations plan webinars, online events, virtual business meetings, conferences and townhalls, consumption and creation of data increases manifold,” said Smrutiranjan Das, ASI Director, IT & Management Systems Business, Vertiv. “To support these increased loads, we are seeing a tremendous growth in the number of edge sites being deployed, and Vertiv CLRA local rack access console is an ideal solution to support local and remote management of IT devices.”

“Digital infrastructure has become the backbone of all organizations, increasingly so after the pandemic hit last year. Businesses are heavily dependent on technology for several process, and managing operations from multiple locations across the country. To make sure we align our offerings with the growing market needs, we have launched Vertiv CLRA local rack access console. It allows businesses to easily manage and have access to different sites,” said Sanjay Zadoo, country manager, channel business, Vertiv India.

Key Benefits
  • Space Savings: Vertiv™ CLRA requires only 1U rack space, even with the addition of the optional, pre-integrated 8 or 16-port KVM. The system eliminates the need for cumbersome and inefficient crash cart access. and allows access to up to 512 servers in a cascading installation with the 16-port KVM.
  • Reduce Downtime: Complete entry point to local servers when needed. Access can be limited to authorized users via login credentials.
  • Ease of Use: High-Definition (1920 x 1080) 18.5” LED panel with full-sized keyboard, touch pad and USB pass through ports provides an optimum computing experience.
  • Easy installation: Tool-less installation design allows Vertiv CLRA to be installed quickly, along with providing durability and strength to Vertiv CLRA construction.
  • Remote management: Vertiv CLRA is compatible with Avocent® DSView management software, for a single point of data center infrastructure management.

For more information on the Vertiv CLRA local rack acess consoles and the full portfolio Vertiv IT management solutions, visit Vertiv.com.

About Vertiv

Vertiv (NYSE: VRT) brings together hardware, software, analytics and ongoing services to ensure its customers’ vital applications run continuously, perform optimally and grow with their business needs. Vertiv solves the most important challenges facing today’s data centers, communication networks and commercial and industrial facilities with a portfolio of power, cooling and IT infrastructure solutions and services that extends from the cloud to the edge of the network. Headquartered in Columbus, Ohio, USA, Vertiv employs approximately 21,000 people and does business in more than 130 countries. For more information, and for the latest news and content from Vertiv, visit Vertiv.com.

Forward-Looking Statements

This release contains forward-looking statements within the meaning of the Private Securities Litigation Reform Act of 1995, Section 27 of the Securities Act, and Section 21E of the Securities Exchange Act. These statements are only a prediction. Actual events or results may differ materially from those in the forward-looking statement set forth herein. Readers are referred to Vertiv’s filings with the Securities and Exchange Commission, including its most recent Annual Report on Form 10-K/A and any subsequent Quarterly Reports on Form 10-Q for a discussion of these and other important risk factors concerning Vertiv and its operations. Vertiv is under no obligation to, and expressly disclaims any obligation to, update or alter its forward-looking statements, whether as a result of new information, future events or otherwise.

 

CONTACT

Ipshita Balu

T  +91 95901 11798

E  ipshita.balu@gmail.com 

PRODUCTS & SERVICES
Partner Login

Language & Location