Sorry, this page isn't available for your location.

The page you're viewing is for English (India) region.

Working with our Vertiv Sales team enables complex designs to be configured to your unique needs. If you are an organization seeking technical guidance on a large project, Vertiv can provide the support you require.

Learn More

Many customers work with a Vertiv reseller partner to buy Vertiv products for their IT applications. Partners have extensive training and experience, and are uniquely positioned to specify, sell and support entire IT and infrastructure solutions with Vertiv products.

Find a Reseller

Already know what you need? Want the convenience of online purchase and shipping? Certain categories of Vertiv products can be purchased through an online reseller.


Find an Online Reseller

Need help choosing a product? Speak with a highly qualified Vertiv Specialist who will help guide you to the solution that is right for you.



Contact a Vertiv Specialist

Sorry, this page isn't available for your location.

The page you're viewing is for English (India) region.

Vertiv Introduces New High Efficiency DC Rectifier in India, Perfect for Growing Telecom Operations and Demanding Environments

September 16, 2021

The Vertiv™ eSure™ rectifier provides adjustable, stable DC voltage and remote control capabilities

Mumbai, India [September 16, 2021] – Vertiv (NYSE: VRT), a global provider of critical digital infrastructure and continuity solutions, today introduced the Vertiv™ eSure™ R48-4300E3A rectifier, a high-efficiency rectifier designed to convert standard AC supply voltages into stable nominal DC voltage that is adjustable to individual application needs. This new offering is available in India now.

The Vertiv eSure is an efficient and reliable rectifier that helps reduce power consumption and lower operating costs, while maintaining reliable power quality and performance. It offers the latest patented switchmode technology and uses digital signalling processor (DSP) functionality to ensure efficient operation. In cases where higher load capacity is required, multiple rectifiers can be connected in parallel to support a variety of telecom applications. And, with many organizations now adopting hybrid models or working entirely from home, rectifier modules can also be managed and controlled remotely, when combined with a Vertiv controller.

With the eSure™ rectifier, organizations can operate their DC plants in the most demanding environments, due to its wide input voltage range. It is also safe and easy to expand capacity and perform maintenance during live system operation, with the hot-pluggable module design. Additionally, with 4.32 kW of full output power up to 45 degrees Celsius, this rectifier is designed to deliver optimum performance at higher ambient temperatures.

“Organizations in India are increasingly focusing on sustainable business strategies. Adopting digital infrastructure that supports this goal has become essential to companies across the board,” said Dinesh Dhut, senior director, DC power / OSP, offering management (India and SEA Market), Vertiv. “Vertiv’s newly launched power rectifier aligns perfectly with today’s business requirements, by reducing power consumption without impacting the reliability of its operation. As organizations enter a new era of hybrid working models, it is important that they are backed by reliable digital infrastructure.”

With a maximum efficiency of up to 96.5%, the eSure™ rectifier can handle maximum AC input of 27A at 176 VAC and a maximum DC output of 81.5A at -53 VDC. It has an inbuilt alarm, signalling system and visual indicators that send reports directly to the system controller. It can operate at an altitude of up to 6560 feet at full power and relative humidity levels of up to 95%. Vertiv eSure rectifiers deliver proven reliability that meets global safety standards.

For more information on Vertiv eSure R48-4300E3A rectifier and other IT management solutions from Vertiv, visit Vertiv.com.

About Vertiv

Vertiv (NYSE: VRT) brings together hardware, software, analytics and ongoing services to ensure its customers’ vital applications run continuously, perform optimally and grow with their business needs. Vertiv solves the most important challenges facing today’s data centers, communication networks and commercial and industrial facilities with a portfolio of power, cooling and IT infrastructure solutions and services that extends from the cloud to the edge of the network. Headquartered in Columbus, Ohio, USA, Vertiv employs approximately 21,000 people and does business in more than 130 countries. For more information, and for the latest news and content from Vertiv, visit Vertiv.com.

Forward-Looking Statements

This release contains forward-looking statements within the meaning of the Private Securities Litigation Reform Act of 1995, Section 27 of the Securities Act, and Section 21E of the Securities Exchange Act. These statements are only a prediction. Actual events or results may differ materially from those in the forward-looking statement set forth herein. Readers are referred to Vertiv’s filings with the Securities and Exchange Commission, including its most recent Annual Report on Form 10-K/A and any subsequent Quarterly Reports on Form 10-Q for a discussion of these and other important risk factors concerning Vertiv and its operations. Vertiv is under no obligation to, and expressly disclaims any obligation to, update or alter its forward-looking statements, whether as a result of new information, future events or otherwise.

 

CONTACT

Aldo Dias
T +91 8108953838
aldo.dias@vertiv.com

PRODUCTS & SERVICES
Overview
PARTNERS
Overview
Consultants Corner
Partner Login

Language & Location