Sorry, this page isn't available for your location.

The page you're viewing is for English (India) region.

Working with our Vertiv Sales team enables complex designs to be configured to your unique needs. If you are an organization seeking technical guidance on a large project, Vertiv can provide the support you require.

Learn More

Many customers work with a Vertiv reseller partner to buy Vertiv products for their IT applications. Partners have extensive training and experience, and are uniquely positioned to specify, sell and support entire IT and infrastructure solutions with Vertiv products.

Find a Reseller

Already know what you need? Want the convenience of online purchase and shipping? Certain categories of Vertiv products can be purchased through an online reseller.


Find an Online Reseller

Need help choosing a product? Speak with a highly qualified Vertiv Specialist who will help guide you to the solution that is right for you.



Contact a Vertiv Specialist

Sorry, this page isn't available for your location.

The page you're viewing is for English (India) region.

Vertiv introduces a compact, double conversion UPS with inbuilt battery for power backup at home and small sites

January 31, 2022

The 1 kVA rated uninterruptible power supply system provides total isolation from the mains for protection from a spectrum of power anomalies

Mumbai, India [December 15, 2021] – Vertiv, (NYSE: VRT), a global provider of critical digital infrastructure and continuity solutions, today introduced the Liebert® GXT MT+ CX4 1K SB, a true double conversion online uninterruptible power supply (UPS) system with an inbuilt battery designed to provide a capacity of 1 kVA.  This solution is available now in India. 

With several organizations going back to a work from home model due to the second wave of COVID-19 in India, UPS systems that support remote working have become a requirement for availability. The resultant increased loads on data centers have also made power back-up solutions critical in supporting business continuity, including increasingly critical small and remote applications. 

Liebert GXT MT+ CX4 1K SB provides complete protection of the load from the mains aberrations, along with an inbuilt battery and a compact design that makes the system ideal to support work-from-home, data networks, small data centers and VOIP applications. The UPS has a 50/60 Hz automatic frequency converter mode and an inbuilt over voltage cutoff device (OVCD). The UPS features a new graphical LCD display which provides UPS status, load level, battery level, input/output voltage and discharge timer. It also automatically sets off alarms in case of any battery malfunctions or overload, and helps in faults diagnostics and trouble shooting. 

Fluctuating input power can impact the operation and health of connected equipment. Data centers and other critical applications require robust and flexible power solutions to help them run round the clock. The Liebert GXT MT+ CX4 1K SB is equipped with true online double conversion with digital signing process (DSP) control technology to ensure high performance and reliability. It has a double conversion efficiency of up to 89% and can adapt to any environment for optimized battery performance. Additionally, the new UPS has an insulated-gate bipolar transistor (IGBT) based rectifier, and has a wide input frequency range compatible with generator operation.

“Digital infrastructure, especially in times of remote working, plays a crucial role in supporting continuity of operations. Hence, being equipped with the right kind of power back-up solutions is of primary importance to organizations and their workforce. At Vertiv, we are committed to providing customized solutions to our customers’ evolving requirements,” said Gopakumar Ambujakshan, director, product management (small and micro UPS), Vertiv in India. “ Since the initial phase of the lockdowns last year, Vertiv has continued to extend its support to businesses by providing power and cooling solutions to ensure business continuity. The Liebert® GXT MT+ CX4 1K SB system is yet another product we have introduced to support the new working environment.” 

For more information on the Liebert GXT MT+ CX4 1K SB and Vertiv’s full portfolio of uninterruptible power supply (UPS) solutions, visit Vertiv.com.

About Vertiv

Vertiv (NYSE: VRT) brings together hardware, software, analytics and ongoing services to ensure its customers’ vital applications run continuously, perform optimally and grow with their business needs. Vertiv solves the most important challenges facing today’s data centers, communication networks and commercial and industrial facilities with a portfolio of power, cooling and IT infrastructure solutions and services that extends from the cloud to the edge of the network. Headquartered in Columbus, Ohio, USA, Vertiv employs approximately 20,000 people and does business in more than 130 countries. For more information, and for the latest news and content from Vertiv, visit Vertiv.com.

Forward-Looking Statements

This release contains forward-looking statements within the meaning of the Private Securities Litigation Reform Act of 1995, Section 27 of the Securities Act, and Section 21E of the Securities Exchange Act. These statements are only a prediction. Actual events or results may differ materially from those in the forward-looking statement set forth herein. Readers are referred to Vertiv’s filings with the Securities and Exchange Commission, including its most recent Annual Report on Form 10-K and any subsequent Quarterly Reports on Form 10-Q for a discussion of these and other important risk factors concerning Vertiv and its operations. Vertiv is under no obligation to, and expressly disclaims any obligation to, update or alter its forward-looking statements, whether as a result of new information, future events or otherwise.

CONTACT

Aldo Dias
T +91 8108953838
aldo.dias@vertiv.com 

PRODUCTS & SERVICES
Overview
PARTNERS
Overview
Consultants Corner
Partner Login

Language & Location