The page you're viewing is for Traditional Chinese (Taiwan) region.

與 Vertiv 製造商的代表合作,即可根據您的特有需求配置複雜的設計。如果您是尋求大型專案技術指導的組織,Vertiv 可以提供您所需的支援。

了解更多

許多客戶都會與 Vertiv 經銷商合作夥伴合作,為 IT 應用程式購買 Vertiv 產品。合作夥伴擁有豐富的訓練和經驗,獨具優勢,能夠使用 Vertiv 產品指定、銷售和支援整個 IT 和基礎設施解決方案。

尋找經銷商

已經知道自己的需求嗎? 想要享受線上購買和宅配的便利性嗎? 某些類別的 Vertiv 產品可以透過線上經銷商購買。


尋找在線經銷商

需要協助選擇產品嗎? 與合格的 Vertiv 專家交談,讓他們協助您找到適合自己的解決方案。



聯絡 Vertiv 專家

The page you're viewing is for Traditional Chinese (Taiwan) region.

Vertiv expands power portfolio with new compact desktop UPS for personal computing, gaming and networking devices

2026年5月6日

The Vertiv™ PowerUPS 100 Standby Series helps protect essential devices and keep connected home, office and small business equipment operating during unexpected power disruptions

COLUMBUS, Ohio [May 5, 2026] – Vertiv (NYSE: VRT), a global leader in critical digital infrastructure, today introduced the Vertiv™ PowerUPS 100 Standby Series, a new generation of compact uninterruptible power supply (UPS) systems designed to help maintain continuity in distributed digital environments, and reduce the impact of unexpected power interruptions on everyday digital activity. In North America, the 120V series is available with lithium-ion and VRLA models across a range of capacities to support desktop and small office applications.

Part of Vertiv’s end-to-end portfolio supporting critical infrastructure from the data center to the edge and desktop, the Vertiv PowerUPS 100 Standby Series delivers dependable battery backup and surge protection in a sleek, space-saving design for personal computers, gaming consoles, smart home devices, wireless networks, retail point-of-sale equipment and AI PCs. 

"For many small businesses, retail sites and connected workspaces, a short power interruption can disrupt transactions, disconnect networks or put data at risk,” said Ramesh Menon, vice president of IT systems solutions at Vertiv. “The Vertiv PowerUPS 100 Standby Series is designed to make dependable power protection easier to deploy where space, budget and simplicity matter — from desktops and workstations to point-of-sale systems and essential network devices.” 

The UPS includes up to eight outlets with a combination of battery backup and surge protection, allowing users to safeguard multiple critical devices simultaneously. Integrated USB-A and USB-C ports provide convenient charging for mobile devices, while the compact, wall-mountable design enables flexible placement in space-constrained environments. 

The series also prioritizes long-term usability and system management. User-replaceable batteries help extend product lifespan and reduce maintenance costs, while compatibility with Vertiv™ Power Assist software enables automated, graceful shutdown of connected systems during extended outages to help protect against data loss and equipment damage. 

Featuring four VRLA models ranging from 500VA / 305W to 1100VA / 670W, as well as two lithium-ion in 350VA / 210W and 400VA / 240W, the Vertiv™ PowerUPS 100 Standby Series offers capacity options for a range of applications. The series is also certified to Energy Star 2.0 requirements, Department of Energy (DOE) efficiency standards, and FCC Part 15 Class B regulations. 

Models are available with a connected equipment protection plan and are backed by a three-year warranty for Valve-Regulated Lead-Acid (VRLA) configurations and a five-year warranty for lithium-ion models, providing reliable power protection for critical electronics. 

For more information about the Vertiv PowerUPS 100 series and Vertiv’s end-to-end portfolio of power and thermal management solutions that extend from the desktop to the edge, visit Vertiv.com.  

About Vertiv

Vertiv (NYSE: VRT) brings together hardware, software, analytics and ongoing services to enable its customers’ vital applications to run continuously, perform optimally and grow with their business needs. Vertiv solves the most important challenges facing today’s data centers, communication networks and commercial and industrial facilities with a portfolio of power, cooling and IT infrastructure solutions and services that extends from the cloud to the edge of the network. Headquartered in Westerville, Ohio, USA, Vertiv does business in more than 130 countries. For more information, and for the latest news and content from Vertiv, visit Vertiv.com. 

Forward-looking statements

This release contains forward-looking statements within the meaning of the Private Securities Litigation Reform Act of 1995, Section 27 of the Securities Act, and Section 21E of the Securities Exchange Act. These statements are only a prediction. Actual events or results may differ materially from those in the forward-looking statements set forth herein. Readers are referred to Vertiv’s filings with the Securities and Exchange Commission, including its most recent Annual Report on Form 10-K and any subsequent Quarterly Reports on Form 10-Q for a discussion of these and other important risk factors concerning Vertiv and its operations. Vertiv is under no obligation to, and expressly disclaims any obligation to, update or alter its forward-looking statements, whether as a result of new information, future events or otherwise. 

CONTACT
Ruder Finn
E 
Vertiv@RuderFinn.com

相關洞察

Battery Backup Image

文章話題

Battery Backup

選擇您的國家/區域和語言