The page you're viewing is for Traditional Chinese (Taiwan) region.

與 Vertiv 製造商的代表合作,即可根據您的特有需求配置複雜的設計。如果您是尋求大型專案技術指導的組織,Vertiv 可以提供您所需的支援。

了解更多

許多客戶都會與 Vertiv 經銷商合作夥伴合作,為 IT 應用程式購買 Vertiv 產品。合作夥伴擁有豐富的訓練和經驗,獨具優勢,能夠使用 Vertiv 產品指定、銷售和支援整個 IT 和基礎設施解決方案。

尋找經銷商

已經知道自己的需求嗎? 想要享受線上購買和宅配的便利性嗎? 某些類別的 Vertiv 產品可以透過線上經銷商購買。


尋找在線經銷商

需要協助選擇產品嗎? 與合格的 Vertiv 專家交談,讓他們協助您找到適合自己的解決方案。



聯絡 Vertiv 專家

The page you're viewing is for Traditional Chinese (Taiwan) region.

DKRZ - The German Climate Computing Centre

2017年8月8日

The German Climate Computing Centre (DKRZ), located in the centre of Hamburg, is renowned by climatologists from around the world.

Here, a team of nearly 80 employees combines technical expertise and special high performance computers to perform complex climate simulations for research purposes. As these simulations require significant computing and data storage capacities, DKRZ has been continuously improving its computing power in order to stay abreast in an evolving and competitive industry. With the installation of a new high performance computing system, Mistral, in summer 2015, DKRZ has seen performance increase twentyfold, at a lower power consumption. The investment into increased computing power and storage capacity has helped to make DKRZ one of the world’s elite computing centres for climate research.

Case Summary
Location:

Hamburg, Germany

Critical Need:

DKRZ was faced with the challenge of upgrading its computing power in an efficient way to ensure reliable and failure-free operations for its new mainframe computer, Mistral. The computer’s energy consumption constantly changes, and can deviate up to 50 percent within fractions of a second. As a result, it was necessary to equip the existing computing centre with a completely new infrastructure, including an uninterruptible power supply (UPS) capable of bridging temporary current fluctuations with ease.

Vertiv Solution:

The Liebert Trinergy Cube configuration at DKRZ is particularly unique. By interconnecting a total of six 400 kVA modules, a single UPS system provides 2400 kVA of power. However, this is only one example of numerous technical advantages which the Liebert Trinergy Cube provides

Download the Case Study

相關洞察

T 系統 Image

案例

T 系統

選擇您的國家/區域和語言