Sorry, this page isn't available for your location.

The page you're viewing is for Portuguese (EMEA) region.

Trabalhar com um representante do fabricante Vertiv permite que os designs complexos sejam configurados de acordo com as suas necessidades únicas. Se for uma organização que procura orientação técnica num projeto de grandes dimensões, a Vertiv pode fornecer o apoio de que necessita.

Saiba mais

Muitos clientes trabalham com um parceiro revendedor Vertiv, para comprar produtos Vertiv para as suas aplicações de IT. Os parceiros têm uma vasta formação e experiência, e estão posicionados de forma única para especificar, vender e apoiar soluções completas de TI e infraestruturas com produtos Vertiv.

Encontrar um revendedor

Já sabe do que precisa? Quer a conveniência da compra e do envio online? Determinadas categorias de produtos Vertiv podem ser adquiridas através de um revendedor online.


Encontre um revendedor on-line

Precisa de ajuda para escolher um produto? Fale com um Especialista Vertiv altamente qualificado que o ajudará a orientar-se para a solução certa para si.



Contacte um Especialista Vertiv

Sorry, this page isn't available for your location.

The page you're viewing is for Portuguese (EMEA) region.

Vertiv™ VR Rack and Vertiv™ Geist rPDU expand portfolio of technologies designed to meet demands at the edge

Southampton, UK [November 5, 2018] – Vertiv today introduced new products to meet the unique challenges of the network edge, including the need for rapid deployment, remote monitoring and management, and end-to-end service. Now available to channel partners and customers across Europe, Middle East and Africa (EMEA), the Vertiv™ VR Rack and Vertiv™ Geist rPDU (rack power distribution units) have been designed to meet the needs of edge deployments.

The launch of these products further expands the Vertiv portfolio of edge solutions. The breadth of product and service choices is critical at the edge, where IT needs may be different from site to site and constantly evolving. A single vendor partner that can provide end-to-end infrastructure solutions and support presents strong value to companies that require edge deployments, but do not have the resources or expertise to sustain this business model.

“We see that the edge is progressively evolving and taking shape under four main archetypes, each with different technology requirements,” says Giordano Albertazzi, president for Vertiv in EMEA. “Our new edge portfolio provides our channel partners and customers with a broad choice of flexible and rapidly deployable solutions to match specific needs and help them own their edge.”

The Vertiv VR Rack is a robust and flexible rack solution that allows for rapid deployment. Eight standard sizes are available, all featuring a frame design that delivers about 2.5 inches of additional useable depth compared to similar sized racks, for ease of installation and maintenance of critical equipment. The rack is complemented by a variety of tool-less accessories to help speed deployment and facilitate rack management.

The new Vertiv Geist rPDUs are available in basic, monitored and switched models, stocked for rapid delivery. Monitored and switched models can monitor input power to plus or minus 1 percent accuracy, in addition to standard readings including amps, volts, watts, kWh and power factor. Switched models have many notable features such as the ability to control input power at each outlet, upgradable functionality to monitor each outlet, and patented U-lock receptacles that lock any cord in place to eliminate unintentional disconnection. Both models have a hot swappable communication module to allow rapid change in the field. All models have the industry’s best 5 year warranty, when registered within 120 days of purchase, and may also be supported by the Vertiv Distribution Assurance Package lifecycle support, which includes startup, installation, repair or replacement, emergency response and other features.

Additional information on the Vertiv VR Rack and Vertiv Geist rPDUs is available at www.VertivCo.com/OwnYourEdge-EMEA. To learn more about other Vertiv offerings, please visit www.VertivCo.com.

About Vertiv

Vertiv brings together hardware, software, analytics and ongoing services to ensure its customers’ vital applications run continuously, perform optimally and grow with their business needs. Vertiv solves the most important challenges facing today’s data centres, communication networks and commercial and industrial facilities with a portfolio of power, cooling and IT infrastructure solutions and services that extends from the cloud to the edge of the network. Headquartered in Columbus, Ohio, USA, Vertiv employs around 20,000 people and does business in more than 130 countries. For more information, and for the latest news and content from Vertiv, visit VertivCo.com

Contact:
Gemma Lingham
T +44 208 618 2812
E gemma.lingham@fhflondon.co.uk

Download Images
Acesso de Partner

Idioma e Localização